This version (02 Jan 2023 14:23) was approved by Jagan M.
Running Average
Description
The RunningAverage block computes the average of N samples. Where N is specified in the CurrentBlockSize text field.
Targets Supported
Name | ADSP-214xx | ADSP-215xx/SC5xx | ADAU145x/146x |
Running Avg | Block | Block | NA |
Pins
Name | Type | Description |
Input0 | Audio | Input channel 0 |
Output
Name | Type | Description |
Output0 | Audio | Output channel 0 |
Configurable Parameters
GUI Parameter Name | Default Value | Range | Function Description |
MaxBlockSizeSet | 1 | 1 -1500 (Depends on the size of memory available) | Specifies the maximum samples for averaging. Change in this value requires a re-compilation |
CurrentBlockSize | 1 | 1 - MaxBlockSizeSet | Number of samples to be averaged. Change in this value requires a re-compilation |
NumChannels | 1 | 15 | Number of input and output channels.Change in this value requires a re-compilation |
DSP Parameters
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
MaxBlockSizeSet | Specifies the maximum samples for averaging | Float |
MaxCurrentBlockSize | Number of samples to be averaged | Float |
OneOverN | Inverse of CurrentBlockSize | Float |
DSP Parameter Computation