Click here to return to the Basic DSP section.
This module applies gain to the input and passes to the output pin. When the module is grown the gain value is separate for each of the inputs. It comes in two versions.
HW slew version shall apply the slew whenever gain parameter is changed to avoid click noise.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | dec- audio | Input Audio |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 1: Output | dec- audio | Output audio with gain. |
The module currently supports growth. Both the control and pins are grown for each growth. Add algorithm functionality is not supported. The figure below shows the module when grown for 5 channels.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Gain* | 1 | -128 to 127.999 | Gain value in linear scale. |
Note: Gain control will be repeated for each channels when grown.
In the case of HW slew version. The slew shape can be chosen by right clicking on the module.
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Gain | MultipleControlGainS300Alg1gain0 | Gain Value in linear scale |
Here,
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Slew Mode | MultipleControlGainHWSelwAlg1slew_mode | HW Slew Mode |
Gain | MultipleControlGainHWSelwAlg1gain0 | Gain Value in linear scale |
Here,
Note: Gain parameter shall be repeated for each channel when the algorithm is grown.