Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sigmastudio:toolbox:basicdsp:log2 [21 Aug 2018 11:49] – Updated for SHARC processors Deepak Raghothamresources:tools-software:sigmastudio:toolbox:basicdsp:log2 [21 Aug 2018 11:53] (current) Deepak Raghotham
Line 53: Line 53:
 ^Name^Format [int/dec] - [control/audio]^Function Description^ ^Name^Format [int/dec] - [control/audio]^Function Description^
 |Pin 0: Log value|decimal(ADAU145x) - control \\ float(ADSP-214xx/ADSP-215xx) - control |log2(input)| |Pin 0: Log value|decimal(ADAU145x) - control \\ float(ADSP-214xx/ADSP-215xx) - control |log2(input)|
-===== Grow Algorithm =====+==== Grow Algorithm ====
 The module supports Add functionality. Growth is not supported.  The module supports Add functionality. Growth is not supported. 
-===== GUI Controls =====+==== GUI Controls====
 None None
-===== DSP Parameter Information ===== +==== DSP Parameter Information ====
 None None
-===== Algorithm Description =====+==== Algorithm Description ====
 log2(x) is implemented as (ln(x) / ln(2)) using the change of base formula. log2(x) is implemented as (ln(x) / ln(2)) using the change of base formula.
-ln(x) is implemented using the taylor series expansion +ln(x) is implemented using the taylor series expansion. 
-===== Supported IC's=====+==== Supported IC's ====
 1. ADSP-213xx \\ 1. ADSP-213xx \\
 2. ADSP-214xx \\ 2. ADSP-214xx \\
 3. ADSP-SC5xx \\ 3. ADSP-SC5xx \\
 4. ADSP-215xx 4. ADSP-215xx
resources/tools-software/sigmastudio/toolbox/basicdsp/log2.1534844961.txt.gz · Last modified: 21 Aug 2018 11:49 by Deepak Raghotham