This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:basicdsp:log2 [21 Aug 2018 11:49] – Updated for SHARC processors Deepak Raghotham | resources:tools-software:sigmastudio:toolbox:basicdsp:log2 [21 Aug 2018 11:53] (current) – Deepak Raghotham | ||
---|---|---|---|
Line 53: | Line 53: | ||
^Name^Format [int/dec] - [control/ | ^Name^Format [int/dec] - [control/ | ||
|Pin 0: Log value|decimal(ADAU145x) - control \\ float(ADSP-214xx/ | |Pin 0: Log value|decimal(ADAU145x) - control \\ float(ADSP-214xx/ | ||
- | ===== Grow Algorithm | + | ==== Grow Algorithm ==== |
The module supports Add functionality. Growth is not supported. | The module supports Add functionality. Growth is not supported. | ||
- | ===== GUI Controls | + | ==== GUI Controls==== |
None | None | ||
- | ===== DSP Parameter Information | + | ==== DSP Parameter Information ==== |
None | None | ||
- | ===== Algorithm Description | + | ==== Algorithm Description ==== |
log2(x) is implemented as (ln(x) / ln(2)) using the change of base formula. | log2(x) is implemented as (ln(x) / ln(2)) using the change of base formula. | ||
- | ln(x) is implemented using the taylor series expansion | + | ln(x) is implemented using the taylor series expansion. |
- | ===== Supported IC's===== | + | ==== Supported IC's ==== |
1. ADSP-213xx \\ | 1. ADSP-213xx \\ | ||
2. ADSP-214xx \\ | 2. ADSP-214xx \\ | ||
3. ADSP-SC5xx \\ | 3. ADSP-SC5xx \\ | ||
4. ADSP-215xx | 4. ADSP-215xx |