Click here to return to the Basic DSP page
The feedback algorithm generates a delay in the signal path and reroutes signal to an input occurring earlier in the path. Note that this block must be used if feedback is required in your design. The standard delay block cannot be used to create feedback systems.
There are two versions of ' Feedback' algorithm.
Generates one sample delay in the signal path and reroutes the signal to an input occurring earlier in the path.
Generates delay equal to one blocksize in the signal path and reroutes the signal to an input occurring earlier in the path.
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Sample Input | decimal- audio | Sample Input signal |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Sample Delayed Output | decimal- audio | Sample Output signal |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Block Input | decimal-audio | Block Input Signal |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Block Delayed Output | decimal- audio | Block Output signal |
None
Grow and Add algorithm are not supported for this module.
None
ADAU145x