Next revision | Previous revision |
resources:tools-software:sigmastudio:toolbox:adialgorithmsresourcetable [25 Jul 2012 21:03] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:adialgorithmsresourcetable [15 Nov 2012 21:03] (current) – Fixed Pitch Transposer links William Jahn |
---|
|Surround & 3D Audio|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/superphat|SuperPhat Spatializer]]|162|162|90|52|Allows for a wider stereo image to be played back from two closely spaced speakers.|ADAU144x, ADAU176x, ADAU1781| | |Surround & 3D Audio|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/superphat|SuperPhat Spatializer]]|162|162|90|52|Allows for a wider stereo image to be played back from two closely spaced speakers.|ADAU144x, ADAU176x, ADAU1781| |
|Surround & 3D Audio|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/phatstereo|Phat-Stereo]]|13|13|5|2|Uses stereo cross-coupling to simulate surround in stereo speakers and other 2-channel situations|ADAU144x, ADAU176x, ADAU1781| | |Surround & 3D Audio|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/phatstereo|Phat-Stereo]]|13|13|5|2|Uses stereo cross-coupling to simulate surround in stereo speakers and other 2-channel situations|ADAU144x, ADAU176x, ADAU1781| |
| |Surround & 3D Audio|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/adisurround|ADI Surround]]|191|191|3462|28|TBD|ADAU144x| |
| |Surround & 3D Audio|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/adivirtual|ADI Virtual]]|176|176|177|48|TBD|ADAU144x, ADAU176x, ADAU1781| |
|Voice Detector|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/voiceactivitydetector|Voice Activity Detector]]|48|48|15|5|Outputs signals to be used by the VAD flag for speech detection. Must be used in conjunction with the VAD flag.|ADAU144x, ADAU176x, ADAU1781| | |Voice Detector|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/voiceactivitydetector|Voice Activity Detector]]|48|48|15|5|Outputs signals to be used by the VAD flag for speech detection. Must be used in conjunction with the VAD flag.|ADAU144x, ADAU176x, ADAU1781| |
|Voice Detector|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/voiceactivitydetector|Voice Activity Detector]] (W/ Accelerator)|84|84|21|11|Improved version of the Voice Activity Detector that has an accelerated reaction time after voice stops being present.|ADAU144x, ADAU176x, ADAU1781| | |Voice Detector|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/voiceactivitydetector|Voice Activity Detector]] (W/ Accelerator)|84|84|21|11|Improved version of the Voice Activity Detector that has an accelerated reaction time after voice stops being present.|ADAU144x, ADAU176x, ADAU1781| |
|Voice Detector|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/vadflag|VAD Flag]]|17|17|7|2|Shows you if there is voice or not and must be used in conjunction with the Voice Activity Detector.|ADAU144x, ADAU176x, ADAU1781| | |Voice Detector|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/vadflag|VAD Flag]]|17|17|7|2|Shows you if there is voice or not and must be used in conjunction with the Voice Activity Detector.|ADAU144x, ADAU176x, ADAU1781| |
|Pitch Modification|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/pitchtransposer|Pitch Transposer]]|76|76|320|4|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x, ADAU176x, ADAU1781| | |Pitch Modification|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/pitchmodification/pitchtransposer|Pitch Transposer]]|76|76|320|4|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x, ADAU176x, ADAU1781| |
|Pitch Modification|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/pitchtransposer|Pitch Transposer]] Data Controlled|76|76|320|3|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x, ADAU176x, ADAU1781| | |Pitch Modification|||[[resources/tools-software/sigmastudio/toolbox/adialgorithms/pitchmodification/pitchtransposer|Pitch Transposer]] Data Controlled|76|76|320|3|Shifts the pitch of the incoming signal by changing its fundamental frequency.|ADAU144x, ADAU176x, ADAU1781| |
|Dynamic Bass||Mono|[[resources/tools-software/sigmastudio/toolbox/adialgorithms/dynamicbassboost|Dynamic Bass Boost]]|46|46|23|40|The Dynamic Bass Boost block provides boost that varies with input-signal level: lower levels require, and receive, more bass than higher levels.|ADAU144x, ADAU176x, ADAU1781| | |Dynamic Bass||Mono|[[resources/tools-software/sigmastudio/toolbox/adialgorithms/dynamicbassboost|Dynamic Bass Boost]]|46|46|23|40|The Dynamic Bass Boost block provides boost that varies with input-signal level: lower levels require, and receive, more bass than higher levels.|ADAU144x, ADAU176x, ADAU1781| |
|Dynamic Bass||Mono|[[resources/tools-software/sigmastudio/toolbox/adialgorithms/dynamicbassboost|Dynamic Bass Boost]] (Add Mono)|46||22|40|This grows the algorithm by adding another channel to the block.|ADAU144x, ADAU176x, ADAU1781| | |Dynamic Bass||Mono|[[resources/tools-software/sigmastudio/toolbox/adialgorithms/dynamicbassboost|Dynamic Bass Boost]] (Add Mono)|46||22|40|This grows the algorithm by adding another channel to the block.|ADAU144x, ADAU176x, ADAU1781| |