This shows you the differences between two versions of the page.
resources:tools-software:sigmastudio:toolbox:adialgorithms:noisereduction [09 Oct 2012 17:51] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:adialgorithms:noisereduction [09 Oct 2012 18:20] (current) – Updated information about GUI Brett Gildersleeve | ||
---|---|---|---|
Line 8: | Line 8: | ||
===Input Pins=== | ===Input Pins=== | ||
^Name^Format [int/dec] - [control/ | ^Name^Format [int/dec] - [control/ | ||
- | |Pin 0: Audio In L|decimal - audio|Audio input| | + | |Pin 0: Audio In|decimal - audio|Audio input| |
===Output Pins=== | ===Output Pins=== | ||
^Name^Format [int/dec] - [control/ | ^Name^Format [int/dec] - [control/ | ||
- | |Pin 0: Audio Out L|decimal - audio|Audio output| | + | |Pin 0: Audio Out|decimal - audio|Audio output| |
===GUI Controls=== | ===GUI Controls=== | ||
^GUI Control Name^Default Value^Range^Function Description^ | ^GUI Control Name^Default Value^Range^Function Description^ | ||
- | |Low Noise Switch|Off|On or Off|Enables the noise reduction algorithm.| | + | |Low Noise Switch|On (red)|On (red) or Off (green)|Enables the noise reduction algorithm. The down (red) setting enables the noise reduction. The up (green) setting will set the algorithm to bypass mode.| |
|Delay|650|300 to 650|Controls the length of the delay path (in samples) of the algorithm. There is some latency required to break the signal into frequency components and make decisions on which bands should be passed through or blocked. Increasing the latency will improve the perceived quality of the audio and noise reduction performance, | |Delay|650|300 to 650|Controls the length of the delay path (in samples) of the algorithm. There is some latency required to break the signal into frequency components and make decisions on which bands should be passed through or blocked. Increasing the latency will improve the perceived quality of the audio and noise reduction performance, | ||
- | |Noise Margin|-30|-30 to -30|This sets the threshold used in the decision making process to determine which bands to pass or block. A higher | + | |Noise Margin|-30|-30 to -30|This sets the threshold used in the decision making process to determine which bands to pass or block. A lower setting will make the noise reduction algorithm more aggressive in blocking signal components. A higher setting will make the noise reduction algorithm a little more " |
===DSP Parameter Information=== | ===DSP Parameter Information=== |