Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Audio In 1 | dec - audio | Mono source audio input |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Audio Out 1 | decimal - audio | Left channel audio output |
Pin 1: Audio Out 2 | decimal - audio | Right channel audio output |
The Mono2Stereo algorithm uses filtering processing to create two separate channels from a single source. There is no user control necessary for this algorithm. The block accepts a single input and the output is a stereo signal.
The following image shows the Mono2Stereo block being used to separate a single source input into a left and right output. The stereo selection Mux allows selection for comparison between the same mono source being sent to left and right versus, the stereo signal from the Mono2Stereo block.
Toolbox Path | ADI Algorithms - Surround & 3D Audio - Mono2Stereo |
Cores Supported | ADAU144x ADAU176x ADAU178x |
“Grow Algorithm” Supported | no |
“Add Algorithm” Supported | no |
Subroutine/Loop Based | no |
Program RAM | 20 |
Data RAM | 33 |
Parameter RAM | 26 |