This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:sigmastudio:toolbox:adialgorithms:automaticspeakereq [09 Nov 2012 20:25] – Added initial content William Jahn | resources:tools-software:sigmastudio:toolbox:adialgorithms:automaticspeakereq [16 Jan 2020 17:29] – Added link to page describing the MLSSA file format KenM | ||
---|---|---|---|
Line 35: | Line 35: | ||
===Source Tab=== | ===Source Tab=== | ||
- | When first opening the control, the source tab will be visible. This is where the response(s) of the desired speakers are loaded. Compatible formats include Impulse Responses with one measurement per line and Frequency responses in the MLSSA format. | + | When first opening the control, the source tab will be visible. This is where the response(s) of the desired speakers are loaded. Compatible formats include Impulse Responses with one measurement per line and Frequency responses in the [[resources: |
\\ | \\ | ||
{{ AutoEQ3.png }} | {{ AutoEQ3.png }} | ||
Line 43: | Line 43: | ||
- **Impulse Response Radio Button** – Click this to use an Impulse Response Measurement as the speaker response. Disables the Frequency Response file import. | - **Impulse Response Radio Button** – Click this to use an Impulse Response Measurement as the speaker response. Disables the Frequency Response file import. | ||
- | - **Frequency Response Radio Button** – Click this to use a Frequency Response Measurement as the speaker response. MLSSA format supported. Disables all Impulse Response related controls. | + | - **Frequency Response Radio Button** – Click this to use a Frequency Response Measurement as the speaker response. |
- Click to load Impulse Response | - Click to load Impulse Response | ||
- Click to load Frequency Response | - Click to load Frequency Response | ||
Line 153: | Line 153: | ||
- **Filter Table** – This displays all the information about each filter. | - **Filter Table** – This displays all the information about each filter. | ||
- **Fixed Checkbox** – This only applies to the initialized filters. Checking this box will make the algorithm “skip over” that filter. It will be applied directly to the transducer without being optimized by the Automatic Speaker EQ algorithm at all. | - **Fixed Checkbox** – This only applies to the initialized filters. Checking this box will make the algorithm “skip over” that filter. It will be applied directly to the transducer without being optimized by the Automatic Speaker EQ algorithm at all. | ||
- | <note important> | + | <WRAP important> |
- | </note> | + | </WRAP> |
===Advanced Settings=== | ===Advanced Settings=== |