This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:adialgorithms:adaptivebeamforming [06 Aug 2012 20:27] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:adialgorithms:adaptivebeamforming [13 Jan 2021 09:07] (current) – Fixed bad link for adau1761_adaptivebeamformingexample.zip Ioana Chelaru | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Adaptive Beam Forming ====== | ====== Adaptive Beam Forming ====== | ||
+ | |||
+ | [[resources: | ||
|The 2-channel SigmaDSP Beamformer uses a modified version of the so-called “Griffiths-Jim” Beamformer (1). This beamformer can track a single source of off-axis interference and place a null in the directional pattern, pointed at the source of the interference. The Block Diagram of this beamformer is shown below.|{{: | |The 2-channel SigmaDSP Beamformer uses a modified version of the so-called “Griffiths-Jim” Beamformer (1). This beamformer can track a single source of off-axis interference and place a null in the directional pattern, pointed at the source of the interference. The Block Diagram of this beamformer is shown below.|{{: | ||
Line 29: | Line 31: | ||
{{ : | {{ : | ||
+ | |||
+ | A downloadable version of this project for the ADAU1761 is available {{ : | ||
===== Pins ===== | ===== Pins ===== | ||