Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sharc-audio-module [05 Aug 2019 15:23] – [SHARC Audio Module Daughter Boards] Chad Wentworthresources:tools-software:sharc-audio-module [14 Oct 2022 20:40] (current) – Change the link to have a more in-line name Rebecca Butler
Line 11: Line 11:
  
 The centerpiece of the SHARC Audio Module is [[http://analog.com|Analog The centerpiece of the SHARC Audio Module is [[http://analog.com|Analog
-Devices']] high-performance [[http://analog.com/sharc|SHARC]] +Devices']] high-performance [[adi>sharc|SHARC]] 
-[[http://analog.com/sc58x|ADSP-SC589]].  Combining two 450 MHz floating point+[[adi>sc58x|ADSP-SC589]].  Combining two 450 MHz floating point
 DSP cores, a 450MHz ARM® Cortex®-A5 core and an FFT/IFFT accelerator with a massive amount DSP cores, a 450MHz ARM® Cortex®-A5 core and an FFT/IFFT accelerator with a massive amount
 of on-board I/O, the ADSP-SC589 is a remarkable engine for audio processing. of on-board I/O, the ADSP-SC589 is a remarkable engine for audio processing.
Line 19: Line 19:
 UART (for MIDI & more), and a [[adi>sigmadsp|SigmaDSP]] 96 kHz, 24-bit audio codec.  A variety of UART (for MIDI & more), and a [[adi>sigmadsp|SigmaDSP]] 96 kHz, 24-bit audio codec.  A variety of
 I/O is provided, including 1/8" stereo jacks, S/PDIF, Gigabit Ethernet, USB OTG I/O is provided, including 1/8" stereo jacks, S/PDIF, Gigabit Ethernet, USB OTG
-& HS as well as Analog Devices' revolutionary [[http://analog.com/a2b|A2B multi channel+& HS as well as Analog Devices' revolutionary [[adi>a2b|A2B multi channel
 audio interface]]. In addition, on the underside of the board are two expansion audio interface]]. In addition, on the underside of the board are two expansion
 connectors (60 pin 0.100 pitch) with access to most of the signals available on connectors (60 pin 0.100 pitch) with access to most of the signals available on
Line 64: Line 64:
   * **[[:resources:tools-software:sharc-audio-module:faust|Faust and the SHARC Audio Module]]** - Provides details about the Faust language and how it integrates with the SHARC Audio Module.    * **[[:resources:tools-software:sharc-audio-module:faust|Faust and the SHARC Audio Module]]** - Provides details about the Faust language and how it integrates with the SHARC Audio Module. 
   * **[[:resources:tools-software:sharc-audio-module:micropython|MicroPython for the SHARC Audio Module]]** - Provides examples and tutorials about how to use MicroPython on the SHARC Audio Module.   * **[[:resources:tools-software:sharc-audio-module:micropython|MicroPython for the SHARC Audio Module]]** - Provides examples and tutorials about how to use MicroPython on the SHARC Audio Module.
 +  * **[[:resources:tools-software:sharc-audio-module:advanced-audio-projects|New and Experimental things for the SHARC Audio Module]]** - Provides examples and tutorials about how to set up and run some new and emerging features of the SHARC Audio Module.
resources/tools-software/sharc-audio-module.txt · Last modified: 14 Oct 2022 20:40 by Rebecca Butler