Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:tools-software:sharc-audio-module:hardware [03 Oct 2018 19:14] – remove redirect Chad Wentworth | resources:tools-software:sharc-audio-module:hardware [19 Apr 2019 22:23] (current) – Dan Ledger |
---|
* **[[:resources:tools-software:sharc-audio-module:hardware:audioproj-fin|Audio Project Fin]]** - Hardware reference guide for the Audio Project Fin that connects to the SHARC Audio Module main board using the expansion interface. | * **[[:resources:tools-software:sharc-audio-module:hardware:audioproj-fin|Audio Project Fin]]** - Hardware reference guide for the Audio Project Fin that connects to the SHARC Audio Module main board using the expansion interface. |
* **[[:resources:tools-software:sharc-audio-module:hardware:class-d|Class-D Amplifier Module]]** - Hardware reference guide for the Class-D Amplifier Module that connects to the SHARC Audio Module main board using the A2B bus. | * **[[:resources:tools-software:sharc-audio-module:hardware:class-d|Class-D Amplifier Module]]** - Hardware reference guide for the Class-D Amplifier Module that connects to the SHARC Audio Module main board using the A2B bus. |
| * **[[:resources:tools-software:sharc-audio-module:hardware:creating|Create your own Fin]]** - Design file templates and guidelines for creating your own SHARC Audio Module Fin board |
---- | ---- |
{{navigation SHARC Audio Module#baremetal|Bare Metal Framework#.|SHARC Audio Module#.faust|Faust and the SHARC Audio Module}} | {{navigation SHARC Audio Module#baremetal|Bare Metal Framework#.|SHARC Audio Module#.faust|Faust and the SHARC Audio Module}} |