This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sharc-audio-module:hardware:main-board [25 Apr 2019 20:17] – [Boot Mode Jumper (JP1)] Chad Wentworth | resources:tools-software:sharc-audio-module:hardware:main-board [20 Oct 2023 21:05] (current) – [Main Differences Between Rev 2.1 and Rev 1.5] Chad Wentworth | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== SHARC Audio Module | + | ====== SHARC Audio Module(Revision 1.5) ====== |
+ | |||
+ | < | ||
The [[adi> | The [[adi> | ||
[[adi> | [[adi> | ||
[[adi> | [[adi> | ||
- | audio codec and an [[adi> | + | audio codec and an [[adi> |
{{: | {{: | ||
Line 10: | Line 12: | ||
**The SHARC Audio Module Main Board** | **The SHARC Audio Module Main Board** | ||
- | {{: | + | {{: |
**Block Diagram of the SHARC Audio Module Main Board** | **Block Diagram of the SHARC Audio Module Main Board** | ||
+ | |||
+ | ===== Main Differences Between Rev 2.1 and Rev 1.5 ===== | ||
+ | < | ||
+ | * Dedicated oscillators have replaced the programmable clock | ||
+ | * Ethernet PHY is now the ADIN1300 | ||
===== Schematics, PCB Layout, Bill of Materials ===== | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | SHARC Audio Module Main Board Rev 1.4 Design and Integration Files | + | SHARC Audio Module Main Board Rev 2.1 Design and Integration Files |
- | * {{ : | + | * {{ : |
- | * {{ : | + | * {{ : |
- | * {{ : | + | * {{ : |
- | * {{ : | + | </ |
+ | |||
+ | <WRAP round download> | ||
+ | SHARC Audio Module Main Board Rev 1.5 Design | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
</ | </ | ||
Line 38: | Line 51: | ||
===== 512Mb SPI Flash ===== | ===== 512Mb SPI Flash ===== | ||
- | A 512Mbit SPI Flash on the SHARC Audio Module | + | A 512Mbit SPI Flash on the SHARC Audio Module |
- | application | + | |
- | MicroSD card. | + | |
===== 10/100/1000 Ethernet ===== | ===== 10/100/1000 Ethernet ===== | ||
The SHARC Audio Module has a 10/100/1000 Ethernet module to provide network and | The SHARC Audio Module has a 10/100/1000 Ethernet module to provide network and | ||
- | internet access to the board. The default IP address for this board, while | + | internet access to the board. |
- | running the official SHARC Audio Module Linux OS is 192.168.1.9. | + | |
===== USB Type A Host Port and USB MicroAB Host/ | ===== USB Type A Host Port and USB MicroAB Host/ | ||
The USB Type A port is Host mode only, and is for USB WiFi, Bluetooth and USB | The USB Type A port is Host mode only, and is for USB WiFi, Bluetooth and USB | ||
- | memory devices. | + | memory devices. The connector is combined with the Ethernet jack. |
The USB MicroAB can be a Host/Device or OTG connection. This interface can be | The USB MicroAB can be a Host/Device or OTG connection. This interface can be | ||
Line 126: | Line 136: | ||
| PD_09| | | PD_09| | ||
- | ===== FTDI Header | + | ===== USB/UART connector |
- | This connector is compatible with most FTDI 3.3v UART to USB adapters. | + | This connector is for USB to UART communication using UART0 on the ADSP-SC589 processor. |
- | + | ||
- | | '' | + | |
- | | '' | + | |
- | | '' | + | |
- | | '' | + | |
- | | '' | + | |
- | | '' | + | |
===== Automotive Audio Bus (A2B) Interface Duraclick (P6, P7) ===== | ===== Automotive Audio Bus (A2B) Interface Duraclick (P6, P7) ===== | ||
Line 141: | Line 144: | ||
The A2B bus uses crossover cables to connect nodes to each other. '' | The A2B bus uses crossover cables to connect nodes to each other. '' | ||
upstream towards the Master Node in the network and '' | upstream towards the Master Node in the network and '' | ||
- | the next slave in the network. The SHARC Audio Module uses the [[adi> | + | the next slave in the network. The SHARC Audio Module uses the [[adi> |
* '' | * '' | ||
Line 197: | Line 200: | ||
===== MicroSD Card Slot (J6) ===== | ===== MicroSD Card Slot (J6) ===== | ||
- | The MicroSD card slot on the SHARC Audio Module | + | The MicroSD card slot on the SHARC Audio Module |
- | that contains the SHARC Audio Module Linux OS. uBoot is flashed | + | |
- | SPI Flash unit and by default will boot into the Linux OS stored on the MicroSD | + | |
- | card. | + | |
===== JTAG Interface (P1) ===== | ===== JTAG Interface (P1) ===== | ||
Line 217: | Line 217: | ||
| 2-3 | '' | | 2-3 | '' | ||
| None | '' | | None | '' | ||
- | |||
- | <note important> | ||
===== Pushbuttons (PB1, PB2) ===== | ===== Pushbuttons (PB1, PB2) ===== | ||