Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sharc-audio-module:hardware:main-board [14 Mar 2019 20:49] – [Schematics, PCB Layout, Bill of Materials] Chad Wentworthresources:tools-software:sharc-audio-module:hardware:main-board [20 Oct 2023 21:05] (current) – [Main Differences Between Rev 2.1 and Rev 1.5] Chad Wentworth
Line 1: Line 1:
-====== SHARC Audio Module Main Board ======+====== SHARC Audio Module(Revision 1.5) ====== 
 + 
 +<note>SHARC Audio Module revision 1.4 hardware reference information can be found at [[resources:tools-software:sharc-audio-module:hardware:main-board:rev1_4|Main Board(Revision 1.4)]]</note>
  
 The [[adi>sharcaudiomodule|SHARC Audio Module]] uses the The [[adi>sharcaudiomodule|SHARC Audio Module]] uses the
 [[adi>sc58x|ADSP-SC589]] [[adi>sharc|SHARC]] processor along with an [[adi>sc58x|ADSP-SC589]] [[adi>sharc|SHARC]] processor along with an
 [[adi>en/products/audio-video/audio-codecs/adau1761.html|ADAU1761]] SigmaDSP [[adi>en/products/audio-video/audio-codecs/adau1761.html|ADAU1761]] SigmaDSP
-audio codec and an [[adi>en/products/ad2425w.html|AD2425W]] [[adi>a2b|A2B]] transceiver in a compact form for audio development.+audio codec and an [[adi>en/products/ad2428w.html|AD2428W]] [[adi>a2b|A2B]] transceiver in a compact form for audio development.
  
 {{:resources:tools-software:sharc-audio-module:hardware:sam-main-board-top.png?direct&600|}} {{:resources:tools-software:sharc-audio-module:hardware:sam-main-board-top.png?direct&600|}}
Line 10: Line 12:
 **The SHARC Audio Module Main Board** **The SHARC Audio Module Main Board**
  
-{{:resources:tools-software:sharc-audio-module:hardware:main-board-diagram.png?nolink&600|}}+{{:resources:tools-software:sharc-audio-module:hardware:main-board-diagram_1.5.png?nolink&600|}}
  
 **Block Diagram of the SHARC Audio Module Main Board** **Block Diagram of the SHARC Audio Module Main Board**
 +
 +===== Main Differences Between Rev 2.1 and Rev 1.5 =====
 +<note>The SHARC Audio Module revision 2.1 main hardware board needs the SHARC Audio Module Bare Metal SDK 2.2.0 software installation.</note>
 +  * Dedicated oscillators have replaced the programmable clock
 +  * Ethernet PHY is now the ADIN1300
  
 ===== Schematics, PCB Layout, Bill of Materials ===== ===== Schematics, PCB Layout, Bill of Materials =====
  
 <WRAP round download> <WRAP round download>
-SHARC Audio Module Main Board Rev 1.Design and Integration Files +SHARC Audio Module Main Board Rev 2.Design and Integration Files 
-  * {{ :resources:tools-software:sharc-audio-module:hardware:a0939-2016.pdf | Schematics}} +  * {{ :resources:tools-software:sharc-audio-module:hardware:a0939-2016_rev2.1.pdf | Schematics}} 
-  * {{ :resources:tools-software:sharc-audio-module:hardware:A0939-2016_BOM.xlsx | Bill of Materials}} +  * {{ :resources:tools-software:sharc-audio-module:hardware:a0939-2016_bom_2_1.xlsx | Bill of Materials}} 
-  * {{ :resources:tools-software:sharc-audio-module:hardware:a0939-2016_1p4.zip | Fabrication and Assembly Files}} +  * {{ :resources:tools-software:sharc-audio-module:hardware:sc589-mini_rev_2.1_design_database.zip | Design Package}} 
-  * {{ :resources:tools-software:sharc-audio-module:hardware:ADZS-SC589-MINI Archive R1.4.zip | Design Package}}  +</WRAP> 
 + 
 +<WRAP round download> 
 +SHARC Audio Module Main Board Rev 1.5 Design and Integration Files 
 +  * {{ :resources:tools-software:sharc-audio-module:hardware:a0939-2016_rev1.5.pdf | Schematics}} 
 +  * {{ :resources:tools-software:sharc-audio-module:hardware:a0939-2016_bom_1_5.xlsx | Bill of Materials}} 
 +  * {{ :resources:tools-software:sharc-audio-module:hardware:adzs-sc589-mini_rev_1.5_design_database.zip | Design Package}}
 </WRAP> </WRAP>
  
Line 38: Line 51:
 ===== 512Mb SPI Flash ===== ===== 512Mb SPI Flash =====
  
-A 512Mbit SPI Flash on the SHARC Audio Module contains preloaded uBoot +A 512Mbit SPI Flash on the SHARC Audio Module that is ready to be programmed with users desired audio application.
-application that will launch the SHARC Audio Module Linux distribution off the +
-MicroSD card.+
  
 ===== 10/100/1000 Ethernet ===== ===== 10/100/1000 Ethernet =====
  
 The SHARC Audio Module has a 10/100/1000 Ethernet module to provide network and The SHARC Audio Module has a 10/100/1000 Ethernet module to provide network and
-internet access to the board. The default IP address for this board, while +internet access to the board.
-running the official SHARC Audio Module Linux OS is 192.168.1.9.+
  
 ===== USB Type A Host Port and USB MicroAB Host/Device/OTG Port ===== ===== USB Type A Host Port and USB MicroAB Host/Device/OTG Port =====
  
 The USB Type A port is Host mode only, and is for USB WiFi, Bluetooth and USB The USB Type A port is Host mode only, and is for USB WiFi, Bluetooth and USB
-memory devices.+memory devices. The connector is combined with the Ethernet jack.
  
 The USB MicroAB can be a Host/Device or OTG connection. This interface can be The USB MicroAB can be a Host/Device or OTG connection. This interface can be
Line 126: Line 136:
 |            PD_09|  ''63''  |  ''64''  |PD_11          | |            PD_09|  ''63''  |  ''64''  |PD_11          |
  
-===== FTDI Header (P8) =====+===== USB/UART connector (P6) =====
  
-This connector is compatible with most FTDI 3.3v UART to USB adapters. +This connector is for USB to UART communication using UART0 on the ADSP-SC589 processor.
- +
-|  ''1''  |GND              | +
-|  ''2''  |PD_00/UART0_CTS +
-|  ''3''  |N/C              | +
-|  ''4''  |PC_14/UART0_RX   | +
-|  ''5''  |PC_13/UART0_TX   | +
-|  ''6''  |PC_15/UART0_RTS  |+
  
 ===== Automotive Audio Bus (A2B) Interface Duraclick (P6, P7) ===== ===== Automotive Audio Bus (A2B) Interface Duraclick (P6, P7) =====
Line 141: Line 144:
 The A2B bus uses crossover cables to connect nodes to each other. ''P6'' connects to The A2B bus uses crossover cables to connect nodes to each other. ''P6'' connects to
 upstream towards the Master Node in the network and ''P7'' connects downstream to upstream towards the Master Node in the network and ''P7'' connects downstream to
-the next slave in the network. The SHARC Audio Module uses the [[adi>en/products/audio-video/automotive-audio-bus/ad2425w.html|AD2425W]] IC.+the next slave in the network. The SHARC Audio Module uses the [[adi>en/products/audio-video/automotive-audio-bus/ad2428w.html|AD2428W]] IC.
  
   * ''BLCK'' is connected to ''DAI0_PIN07''   * ''BLCK'' is connected to ''DAI0_PIN07''
Line 182: Line 185:
  
   * SPDIF Input is connected to ''DAI0_PIN19''.   * SPDIF Input is connected to ''DAI0_PIN19''.
-  * SPDIF Output is connected to ''DAI0_PIIN20''.+  * SPDIF Output is connected to ''DAI0_PIN20''.
  
 ===== USBi Connector (P2) ===== ===== USBi Connector (P2) =====
Line 197: Line 200:
 ===== MicroSD Card Slot (J6) ===== ===== MicroSD Card Slot (J6) =====
  
-The MicroSD card slot on the SHARC Audio Module is used for the MicroSD card +The MicroSD card slot on the SHARC Audio Module can be used to store the Linux OS as well as other data.
-that contains the SHARC Audio Module Linux OS. uBoot is flashed to the onboard +
-SPI Flash unit and by default will boot into the Linux OS stored on the MicroSD +
-card.+
  
 ===== JTAG Interface (P1) ===== ===== JTAG Interface (P1) =====
Line 215: Line 215:
 ^ Jumper on Pins ^ Boot Mode ^ ^ Jumper on Pins ^ Boot Mode ^
 | 1-2            | ''SPI Boot''  | | 1-2            | ''SPI Boot''  |
-| 2-3            | ''UART Boot ''|+| 2-3            | ''UART Boot'' |
 | None           | ''No Boot''   | | None           | ''No Boot''   |
- 
 ===== Pushbuttons (PB1, PB2) ===== ===== Pushbuttons (PB1, PB2) =====
  
resources/tools-software/sharc-audio-module/hardware/main-board.txt · Last modified: 20 Oct 2023 21:05 by Chad Wentworth