This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:sharc-audio-module:hardware:class-d [13 Feb 2020 18:46] – [+12v Input Power Jack (P3)] Chad Wentworth | resources:tools-software:sharc-audio-module:hardware:class-d [03 Mar 2020 18:47] – Chad Wentworth | ||
---|---|---|---|
Line 73: | Line 73: | ||
Two GPIO pushbuttons are provided on the A< | Two GPIO pushbuttons are provided on the A< | ||
- | * '' | + | * '' |
- | * '' | + | * '' |
===== GPIO LEDs (LED1, LED2) ===== | ===== GPIO LEDs (LED1, LED2) ===== | ||
Line 80: | Line 80: | ||
There are two GPIO-controlled LEDs on the A< | There are two GPIO-controlled LEDs on the A< | ||
- | * '' | + | * '' |
- | * '' | + | * '' |
===== PDM/TDM Connectors ===== | ===== PDM/TDM Connectors ===== |