This is an old revision of the document!
Using the bare metal project wizard:
No other options need to be changed.
A tremolo is a classic audio effect whereby we modulate the volume, or amplitude, of our audio signal using an oscillator. Here's a nice explanation of how the tremolo effect works and its various parameters.
In this tutorial, we're going to start by building a basic tremolo effect. We'll then add a few additional bells and whistles. Before you begin this tutorial, it's recommended to quickly go through Tutorial: Basic Volume Control.
Just like last time, we'll be working in the callback_audio_processing.cpp
file. We can implement this code either on SHARC core 1 or SHARC core 2.
To begin, we'll build a tremolo effect that relies on fixed parameters just like we did with volume.
#pragma optimize_for_speed void processaudio_callback( ) { static float tremolo_rate = 0.5; // the rate of our tremolo (0.0 to 1.0) static float tremolo_depth = 0.5; // the depth of our tremolo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations // Otherwise, perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample float trem_factor = 1.0 - (tremolo_depth*(0.5*sinf(t)+0.5)); // Update t based on rate and a scalar that gets maps our rate roughly between 1Hz and about 20Hz t += (tremolo_rate * 0.002); // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = trem_factor * audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = trem_factor * audiochannel_0_right_in[i]; } }
Now we will map the HADC0 pot to our rate parameter and the HADC1 pot to our depth parameter. We don't want our rate to drop down to 0.0 since we'd effectively be multiplying our audio by a constant value at some point along the sine wave we're using to modulate. So we'll map the HADC0 input from a value of 0.1 to 1.0 rather than 0.0 to 1.0.
#pragma optimize_for_speed void processaudio_callback( ) { float tremolo_rate = 0.1 + 0.9*multicore_data->audioproj_fin_pot_hadc0; // the rate of our tremolo (0.1 to 1.0) float tremolo_depth = multicore_data->audioproj_fin_pot_hadc1; // the depth of our tremolo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations // Otherwise, perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample float tremolo_factor = 1.0 - (tremolo_depth*(0.5*sinf(t)+0.5)); // Update t based on rate and a scalar that gets maps our rate roughly between 1Hz and about 20Hz t += (tremolo_rate * 0.002); // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = tremolo_factor * audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = tremolo_factor * audiochannel_0_right_in[i]; } }
We may not want the tremolo enabled all the time so let's use one of the buttons on the Audio Project Fin to enable / disable the tremolo effect. Each of the buttons on the Audio Project Fin is mapped to a default callback that can be found in Callback_Pushbuttons.cpp
in the ARM core (<PROJECT_NAME>_core0
). In these callbacks, the LED below each button is toggled by default and a field in the multicore memory structure is written to indicate that a button event has happened. The nice thing is that we don't need to change any of this default pushbutton callback behavior to use SW1 to enable / disable our effect.
In our audio callback, we'll add a new variable called tremolo_enabled
which will be set to false initially. At the bottom of this callback, we'll check to see if SW1/PB_1 has been pressed and if so, we'll toggle the tremolo_enabled
. When it comes time to process the input buffers, we'll check to see if tremolo_enabled is true. If so, we'll apply the effect and if not, we'll just pass the audio through.
#pragma optimize_for_speed void processaudio_callback( ) { float tremolo_rate = 0.1 + 0.9*multicore_data->audioproj_fin_pot_hadc0; // the rate of our tremolo (0.1 to 1.0) float tremolo_depth = multicore_data->audioproj_fin_pot_hadc1; // the depth of our tremolo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations static bool tremolo_enabled = false; // Otherwise, perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample float tremolo_factor = 1.0 - (tremolo_depth*(0.5*sinf(t)+0.5)); // Update t based on rate and a scalar that gets maps our rate roughly between 1Hz and about 20Hz t += (tremolo_rate * 0.002); // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // If tremolo is enabled, apply the effect if (tremolo_enabled) { // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = tremolo_factor * audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = tremolo_factor * audiochannel_0_right_in[i]; // Otherwise, just pass the audio through } else { audiochannel_0_left_out[i] = audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = audiochannel_0_right_in[i]; } } // If a push button event was logged, clear the event and toggle our enable variable if (multicore_data->audioproj_fin_sw_1_core1_pressed) { multicore_data->audioproj_fin_sw_1_core1_pressed = false; tremolo_enabled = !tremolo_enabled; } }
Some more advanced tremolo pedals allow you to repeatedly tap a button at the desired tempo or rate of the effect. We'll use SW2 to allow the user to set the rate of the tremolo by tapping SW2 at the desired tempo.
To do this, we'll add some code to our background loop. This loop is called repeatedly when we're not in the processaudio_callback routine.
void processaudio_background_loop( ) { // ******************************************************************************* // Add any custom background processing here // ******************************************************************************* static uint64_t last_press_cyclecounter = 0; if (multicore_data->audioproj_fin_sw_2_core1_pressed) { multicore_data->audioproj_fin_sw_2_core1_pressed = false; // Use the SHARC cycle counter to measure the time between taps uint64_t current_cyclecounter = __builtin_emuclk(); float delta_seconds = ((float) (current_cyclecounter - last_press_cyclecounter)) * (1.0/(float)CORE_CLOCK_FREQ_HZ); float delta_samples = delta_seconds * AUDIO_SAMPLE_RATE; // If the time between button taps is between 1/20th of a second and 5 seconds, update our tremolo rate if (delta_samples < AUDIO_SAMPLE_RATE * 5.0 && delta_samples > AUDIO_SAMPLE_RATE / 20.0) { tremolo_rate = 6.28318531/delta_samples; } // Update our cycle counter variable last_press_cyclecounter = current_cyclecounter; } }
We'll also need to make two small modifications to our callback. First, we're going to declare tremolo_rate
as a global variable. And, we're going to update the line where we increment our t
variable.
// declared as a global variable so we can modify from processaudio_background_loop() float tremolo_rate = 0.5; #pragma optimize_for_speed void processaudio_callback( ) { float tremolo_depth = multicore_data->audioproj_fin_pot_hadc1; // the depth of our tremolo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations static bool tremolo_enabled = false; // Otherwise, perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample float trem_factor = 1.0 - (tremolo_depth*(0.5*sinf(t)+0.5)); // Update t based on rate and a scalar that gets maps our rate roughly between 1Hz and about 20Hz t += tremolo_rate; // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // If tremolo is enabled, apply the effect if (tremolo_enabled) { // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = trem_factor * audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = trem_factor * audiochannel_0_right_in[i]; // Otherwise, just pass the audio through } else { audiochannel_0_left_out[i] = audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = audiochannel_0_right_in[i]; } } // If a push button event was logged, clear the event and toggle our enable variable if (multicore_data->audioproj_fin_sw_1_core1_pressed) { multicore_data->audioproj_fin_sw_1_core1_pressed = false; tremolo_enabled = !tremolo_enabled; } }