This is an old revision of the document!
Using the bare metal project wizard:
No other options need to be changed.
A ring modulator is a wild audio effect that generates some very interesting sounds. In this effect, we multiply the incoming audio signal using an oscillator. Here's a nice explanation of how the ring modular effect works and its various parameters.
In this tutorial, we're going to start by building a basic ring modulator effect. We'll then add a few additional bells and whistles. Before you begin this tutorial, it's recommended to quickly go through Tutorial: Basic Volume Control.
Just like last time, we'll be working in the callback_audio_processing.cpp
file. We can implement this code either on SHARC core 1 or SHARC core 2.
Just like in the tremelo tutorial, we'll start with some fixed parameters. ringmod_rate
will set the frequency of the sine wave we're using to modulate the signal. ringmod_blend
will set the mix of clean and modulated audio.
void processaudio_callback( ) { static float ringmod_rate = 0.5; // the rate of our ring modulator (0.0 to 1.0) static float ringmod_blend = 0.5; // the blend or mix of our tremelo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations // Otherwise, perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample float ring_factor = sinf(t); // Update t based on rate and a scalar to map into a nice range t += (ringmod_rate * 0.02); // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = (1.0-ringmod_blend)*audiochannel_0_left_in[i] + ringmod_blend*ring_factor*audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = (1.0-ringmod_blend)*audiochannel_0_right_in[i] + ringmod_blend*ring_factor*audiochannel_0_right_in[i]; } }
Now we will map the HADC0 pot to our rate parameter and the HADC1 pot to our blend / mix parameter. In the case, we're mapping HADC0 to a set of values between 2.0 and 6.0 which gives us a nice wide range of frequencies.
void processaudio_callback( ) { float ringmod_rate = 2.0 + 4.0*multicore_data->audioproj_fin_pot_hadc0; // frequency scaler of our ring modulator (2 to 6.0) float ringmod_blend = multicore_data->audioproj_fin_pot_hadc1; // the blend or mix of our tremelo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations // Perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample float ring_factor = sinf(t); // Update t based on rate and a scalar to map into a nice range t += (ringmod_rate * 0.02); // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = (1.0-ringmod_blend)*audiochannel_0_left_in[i] + ringmod_blend*ring_factor*audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = (1.0-ringmod_blend)*audiochannel_0_right_in[i] + ringmod_blend*ring_factor*audiochannel_0_right_in[i]; } }
Some ring modulator pedals allow the user to select between different waveforms to use to modulate the original signal. In this version, we'll use SW2 to select between a sine wave, a triangle wave and a square wave. And SW1 will be used to toggle the effect on and off.
float square_wave( float t ) { float x = sinf(t); if (x >= 0.0) return 1.0; else return -1.0; } float triangle_wave( float t ) { return asinf(cosf(t))/1.57079633; } #pragma optimize_for_speed void processaudio_callback( ) { float ringmod_rate = 2.0 + 4.0*multicore_data->audioproj_fin_pot_hadc0; // frequency scaler of our ring modulator (2 to 6.0) float ringmod_blend = multicore_data->audioproj_fin_pot_hadc1; // the blend or mix of our tremelo (0.0 to 1.0) static float t = 0.0; // current value of t for sine calculations static uint8_t current_modulator = 0; static bool ringmod_enabled = false; // Perform our C-based block processing here! for (int i=0;i<AUDIO_BLOCK_SIZE;i++) { // Calculate our modulation factor for this sample depending on which modulator is selected float ring_factor; if (current_modulator == 0) { ring_factor = sinf(t); } else if (current_modulator == 1) { ring_factor = triangle_wave(t); } else if (current_modulator == 2) { ring_factor = square_wave(t); } // Update t based on rate and a scalar to map into a nice range t += (ringmod_rate * 0.02); // Wrap t if necessary if (t > 6.28318531) t -= 6.28318531; // If ringmod enabled, apply the effect if (ringmod_enabled) { // Multiply each incoming sample by our amplitude modulation value for this sample audiochannel_0_left_out[i] = (1.0-ringmod_blend)*audiochannel_0_left_in[i] + ringmod_blend*ring_factor*audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = (1.0-ringmod_blend)*audiochannel_0_right_in[i] + ringmod_blend*ring_factor*audiochannel_0_right_in[i]; // Otherwise, just pass the audio through } else { audiochannel_0_left_out[i] = audiochannel_0_left_in[i]; audiochannel_0_right_out[i] = audiochannel_0_right_in[i]; } } // Use SW1 / PB_1 to toggle the effect if (multicore_data->audioproj_fin_sw_1_core1_pressed) { multicore_data->audioproj_fin_sw_1_core1_pressed = false; ringmod_enabled = !ringmod_enabled; } // Use SW2 / PB_2 to cycle through the modulating waveforms if (multicore_data->audioproj_fin_sw_2_core1_pressed) { multicore_data->audioproj_fin_sw_2_core1_pressed = false; current_modulator += 1; if (current_modulator >= 3) { current_modulator = 0; } } }
When we press SW2, the LED next to the push button toggles. To disable this behavior, open Callback_Pushbuttons.cpp
in the <PROJECT_NAME>_core0
project. Locate the callback for PB2 (SW2) on the Audio Project Fin and comment out the code to toggle the LED:
// Call back for PB2 on SHARC Audio Module Audio Project Fin void pushbutton_callback_external_2( void * data_object ) { /* static bool sw2_state = false; // Toggle the LED below the button to indicate state sw2_state = !sw2_state; if (sw2_state) { gpio_write(GPIO_AUDIOPROJ_FIN_LED_SW2, GPIO_HIGH); } else { gpio_write(GPIO_AUDIOPROJ_FIN_LED_SW2, GPIO_LOW); } */ // Update our multicore structure to let the SHARCs know that a PB has been pressed multicore_data->audioproj_fin_sw_2_core1_pressed = true; multicore_data->audioproj_fin_sw_2_core2_pressed = true; // Add custom code here }