This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sharc-audio-module:baremetal:project-wizard [14 Nov 2018 02:47] – Chad Wentworth | resources:tools-software:sharc-audio-module:baremetal:project-wizard [01 Feb 2022 15:29] (current) – [Bare Metal Project Wizard] Chad Wentworth | ||
---|---|---|---|
Line 1: | Line 1: | ||
===== Bare Metal Project Wizard ====== | ===== Bare Metal Project Wizard ====== | ||
- | <WRAP 65% tip> | + | |
- | Useful video: [[https:// | + | |
- | </ | + | |
The SHARC Audio Module Bare Metal Project wizard allows you to create a new project configuration for your SHARC Audio Module. | The SHARC Audio Module Bare Metal Project wizard allows you to create a new project configuration for your SHARC Audio Module. | ||
+ | |||
+ | {{youtube> | ||
To begin, open the wizard by selecting **File → New → SHARC Audio Module Bare Metal Project** from the pull-down menu. The **General Project Information** page will appear. This is where a name is given to the new project. Then click Next. | To begin, open the wizard by selecting **File → New → SHARC Audio Module Bare Metal Project** from the pull-down menu. The **General Project Information** page will appear. This is where a name is given to the new project. Then click Next. | ||
+ | <WRAP round 80% important> | ||
+ | If the Bare Metal Framework Wizard does not currently show in CCES under **File → New → SHARC Audio Module Bare Metal Project** does not show, try clicking **File → New → Other** and it should show under the C/C++ tab. This is normally a result of installing a new version of CCES after the Bare Metal Framework has been installed. | ||
+ | </ | ||
==== General Project Information Page ===== | ==== General Project Information Page ===== | ||
{{: | {{: |