This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sharc-audio-module:baremetal:downloading-and-installing [18 Jan 2019 18:44] – Chad Wentworth | resources:tools-software:sharc-audio-module:baremetal:downloading-and-installing [03 Jan 2021 21:43] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 15: | Line 15: | ||
- After completing this operation, you should see three folders appear in the Project Explorer. Each project corresponds to each of the three cores on the ADSP-SC589. Core 0 is the ARM core. Cores 1 and 2 are the two SHARC cores. By default, the project is configured to pass audio from the 1/8" audio input jack to the 1/8" audio output jack. Build the project and create a debug profile for the JTAG emulator you’re using (ICE1000 or ICE2000). From here, you’ll be able to download and run the project on the ADSP-SC589. | - After completing this operation, you should see three folders appear in the Project Explorer. Each project corresponds to each of the three cores on the ADSP-SC589. Core 0 is the ARM core. Cores 1 and 2 are the two SHARC cores. By default, the project is configured to pass audio from the 1/8" audio input jack to the 1/8" audio output jack. Build the project and create a debug profile for the JTAG emulator you’re using (ICE1000 or ICE2000). From here, you’ll be able to download and run the project on the ADSP-SC589. | ||
< | < | ||
- | * For more information on connecting an emulator, see the [[http:// | + | * For more information on connecting an emulator, see the [[adi>media/ |
- | * For more information on setting up the debug profile, see [[http:// | + | * For more information on setting up the debug profile, see [[adi>en/ |
< | < | ||