This is an old revision of the document!
ADI maintains a set of tools to model, interface, and target with ADI RF and microwave devices within MATLAB and Simulink. These are combined into single Toolbox which contains a set of Board Support Packages (BSP). The list of supported boards is provided below.
The current stable Toolbox can be downloaded from the RF Microwave Toolbox GitHub Release Page. Download the latest mltbx file then open that file within MATLAB. Opening the file will automatically install the Toolbox, adding the necessary components to your MATLAB path. The “Analog Devices, Inc. RF Microwave Toolbox” will appear in your Add-Ons Explore within MATLAB.
To interface and stream data with hardware will require installation of libiio and one of two Hardware Support Packages from MathWorks. The libiio library can be obtained on the Github page of the project.
Installation of either:
is required to use the streaming system objects or blocks. These support packages provide the necessary libIIO MATLAB bindings used by ADI's system objects.
The toolbox can only be built under Linux or with Cygwin on a Windows platform. Conveniently, the entire process is automated with a Makefile located in the CI/scripts folder of the repository. The following is required on the system before the build process can be run:
First clone the repo and move into it:
git clone https://github.com/analogdevicesinc/RFMicrowaveToolbox.git cd RFMicrowaveToolbox
To build the toolbox run the following:
make -C CI/scripts build
To create a installable tlbx file run:
make -C CI/scripts gen_tlbx