This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:product-support-software:ad717x_ad411x_mbed_example [27 Dec 2022 08:02] – Janani Sunil | resources:tools-software:product-support-software:ad717x_ad411x_mbed_example [27 Dec 2022 09:23] – Janani Sunil | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD717x/ | + | ====== AD717x/ |
===== Introduction ===== | ===== Introduction ===== | ||
Line 20: | Line 20: | ||
- | //*Note:The firmware provides a basic user-interface for interacting with the evaluation-board. All the main functionality of the AD411x/ | + | //*Note:The firmware provides a basic user-interface for interacting with the evaluation-board. All the main functionality of the AD411x/ |
- | This firmware can support the following members of the AD711x/ | + | |
+ | |||
+ | ====== Useful links====== | ||
+ | {{section> | ||
+ | * [[/ | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
Line 35: | Line 38: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
- | |||
- | ====== Useful links====== | ||
- | {{section> | ||
- | * [[/ | ||
===== Hardware Connections ===== | ===== Hardware Connections ===== |