This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:mbed-user-guide [29 Jun 2016 12:33] – [Step 6 - Download and install GNU ARM Eclipse OpenOCD debugger] Adrian Suciu | resources:tools-software:mbed-user-guide [26 Oct 2016 16:08] (current) – Adrian Suciu | ||
---|---|---|---|
Line 75: | Line 75: | ||
If all the paths were set, the build process should conclude with the following message | If all the paths were set, the build process should conclude with the following message | ||
- | {{ : | + | {{ : |
+ | If the mbed board is connected to the PC, a new drive should appear labeled NODE-F411RE(for STNucleo F411RE). Copy the .bin file that was created after running "make all" to this drive. The bin file will be flashed to the board. | ||
- | ==== Step 5 - Download Eclipse and Java Runtime Environment ==== | + | {{ : |
+ | |||
+ | The quickest way to do this, after "make all" run the "copy < | ||
+ | {{ : | ||
+ | |||
+ | ==== Step 5 - (Nucleo Specific) ==== | ||
+ | |||
+ | Connect the STNucleo board to the PC. | ||
+ | Upgrade the firmware using the following guide: https:// | ||
+ | |||
+ | ==== Step 6 - Download Eclipse and Java Runtime Environment ==== | ||
Download and install the latest Eclipse version from http:// | Download and install the latest Eclipse version from http:// | ||
Line 85: | Line 96: | ||
http:// | http:// | ||
- | ==== Step 6 - Download and install GNU ARM Eclipse plugins and OpenOCD debugger ==== | + | ==== Step 7 - Download and install GNU ARM Eclipse plugins and OpenOCD debugger ==== |
Open Eclipse, go to Help-> Eclipse Marketplace. Search for GNU ARM Eclipse and click install on the first result. This The options should have the OpenOCD plugin checked. After installation is successful close Eclipse. | Open Eclipse, go to Help-> Eclipse Marketplace. Search for GNU ARM Eclipse and click install on the first result. This The options should have the OpenOCD plugin checked. After installation is successful close Eclipse. | ||
Line 94: | Line 105: | ||
Additional information can be found at http:// | Additional information can be found at http:// | ||
- | |||
- | ==== Step 7 - (Nucleo Specific) ==== | ||
- | |||
- | Connect the STNucleo board to the PC. | ||
- | Upgrade the firmware using the following guide: https:// | ||
==== Step 8 - Importing, building and debugging the project. ==== | ==== Step 8 - Importing, building and debugging the project. ==== |