This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linuxdsp:releasenotes [03 Jan 2021 21:43] – fix links Robin Getz | resources:tools-software:linuxdsp:releasenotes [10 Nov 2021 13:24] – David Gibson | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Yocto Linux for ADSP-SC5xx Processors - Release 1.0.0: | + | ====== Yocto Linux for ADSP-SC5xx Processors - Release Notes ====== |
- | + | The following | |
- | ===== Introduction ===== | + | |
- | The Yocto Linux for ADSP-SC5xx Processors product is a new software product that provides users with a Yocto based Linux solution for supported ADSP-SC5xx processors. | + | |
- | This product will replace the Linux Add-In for CrossCore Embedded Studio as the active Linux product for ADSP-SC5xx processors. Note that there is no direct upgrade path for projects that use the Linux Add-In. Please see the **Notable Changes from the Linux Add-In Product** for more details. | + | |
- | + | ||
- | ===== Supported Linux Distributions ===== | + | |
- | The Yocto Linux for ADSP-SC5xx processors product is formally supported on **Ubuntu 18.04 LTS 64-bit**. | + | |
- | While the product will likely build on other modern Linux distributions, | + | |
- | + | ||
- | ===== Supported Processors and EZ-KITs | + | |
- | The following | + | |
- | + | ||
- | <note important> | + | |
- | ^ Development Board ^ Supported Revision | + | |
- | | [[adi> | + | |
- | | [[adi> | + | |
- | | [[adi> | + | |
- | | [[resources/ | + | |
- | + | ||
- | + | ||
- | ===== System Requirements ===== | + | |
- | The following system requirements are recommended: | + | |
- | * Modern multi-core CPU | + | |
- | * 8GB RAM | + | |
- | * At least 60GB of disk space | + | |
- | For installation on the development board your host PC will require: | + | |
- | * Two open USB ports | + | |
- | + | ||
- | Note: The Yocto Linux product is built from source. For improved performance we recommend at least 4 cores and a SSD disk. | + | |
- | ===== Obtaining Technical Support ===== | + | |
- | You can reach Analog Devices software and tools technical support in the following ways: | + | |
- | * Post your questions in the software and development tools support community at [[|https:// | + | |
- | * E-mail your questions about processors and processor applications to processor.support@analog.com | + | |
- | * Submit your questions to technical support directly via http:// | + | |
- | * Contact your Analog Devices sales office or authorized distributor | + | |
- | + | ||
- | ===== New Features And Changes ===== | + | |
- | This is the first release of the Yocto Linux for ADSP-SC5xx Processors product. | + | |
- | + | ||
- | ==== Notable Changes from the Linux Add-In Product ==== | + | |
- | The following major changes have occurred since the last release of the Linux Add-In for Cross-Core Embedded Studio: | + | |
- | * Replaced Buildroot build system with Yocto (version Thud) | + | |
- | * Upgraded Linux kernel from 4.04 to 4.19 LTS | + | |
- | * Replaced corectrl utility with Linux kernel remoteproc feature | + | |
- | * Improved stability for MCAPI multi-core message passing | + | |
- | * Binary images are no longer provided by Analog Devices | + | |
- | + | ||
- | ===== Known Issues ===== | + | |
- | The following issues are known for this release: | + | |
- | * Limited MCAPI support: | + | |
- | * SHARC core control: An issue exists where by attempting to halt the SHARC cores from Linux, the SHARC core may end in a hung state and will not be able to be restarted again from Linux. | + | |
- | * ADSP-SC584 EZ-Kit does not support the Video Decoder and Encoder EI3 Extender Board. This is a limitation of the EZ-Kit. Driver support is provided and this extender board may be used with custom hardware which can support the board. | + | |
- | * ADSP-SC573 does not support the WVGA/LCD EI3 Extender Board. This is a limitation of the EZ-Kit. Driver support is provided and the extender may be used with a compatible custom board. | + | |
- | * ADSP-SC573 EZ-KIT is only supported for BOM versions >= 1.8. Due to issues with the SD Card support, the ADSP-SC573 port in this release will only be supported on versions of the ADSP-SC573 EZ-KIT whose BOM version is at least 1.8. The BOM version is recorded on the underside of the EZ-KIT on a square white sticker. | + | |
- | * SD Card and Rotary can't work simultaneously on ADSP-SC573 EZ-KIT. This is a limitation of the multiplexing pin conflict of the EZ-Kit. Rotary is disabled by default out of box on ADSP-SC573 EZ-KIT. | + | |
- | * QT, Mplayer and Bluetooth ALSA for all processors are not support in this release. | + | |
+ | * [[resources: | ||
+ | * [[resources: | ||
\\ | \\ | ||
---- | ---- | ||
**HOME PAGE: ** [[resources/ | **HOME PAGE: ** [[resources/ |