Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:tools-software:linuxdsp:docs:quickstartguide:source-setup [24 Jul 2020 04:54] – Sunny Feng | resources:tools-software:linuxdsp:docs:quickstartguide:source-setup [24 Jul 2020 05:01] (current) – Sunny Feng |
---|
| |
The following ADI managed repositories are used for the development of Linux for SC5xx: | The following ADI managed repositories are used for the development of Linux for SC5xx: |
| |<100% 46% 18% 18% 18%>| |
^URL ^ Description ^ Latest Development Branch ^ Latest Release Branch ^ | ^URL ^Description ^Latest Development Branch ^Latest Release Branch ^ |
|https://github.com/analogdevicesinc/lnxdsp-adi-meta | ADI Yocto meta layer| develop/yocto-1.0.0| N/A | | |https://github.com/analogdevicesinc/lnxdsp-adi-meta |ADI Yocto meta layer |develop/yocto-1.0.0 |release/yocto-1.0.0 | |
|https://github.com/analogdevicesinc/lnxdsp-repo-manifest| Google repo manifest| develop/yocto-1.0.0| N/A | | |https://github.com/analogdevicesinc/lnxdsp-repo-manifest |Google repo manifest |develop/yocto-1.0.0 |release/yocto-1.0.0 | |
|https://github.com/analogdevicesinc/lnxdsp-scripts | ADI scripts | develop/yocto-1.0.0| N/A | | |https://github.com/analogdevicesinc/lnxdsp-scripts |ADI scripts |develop/yocto-1.0.0 |release/yocto-1.0.0 | |
|https://github.com/analogdevicesinc/u-boot-sharc | U-Boot Bootloader | develop/yocto-1.0.0| N/A | | |https://github.com/analogdevicesinc/u-boot-sharc |U-Boot Bootloader |develop/yocto-1.0.0 |release/yocto-1.0.0 | |
|https://github.com/analogdevicesinc/lnxdsp-linux | Linux kernel | develop/yocto-1.0.0| N/A | | |https://github.com/analogdevicesinc/lnxdsp-linux |Linux kernel |develop/yocto-1.0.0 |release/yocto-1.0.0 | |
|https://github.com/analogdevicesinc/lnxdsp-examples | ADI SHARC examples | develop/yocto-1.0.0| | |https://github.com/analogdevicesinc/lnxdsp-examples |ADI SHARC examples |develop/yocto-1.0.0 |release/yocto-1.0.0 | |
| |
\\ | \\ |