Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:linuxdsp:docs:quickstartguide:sharc-alsa-example [15 Oct 2021 16:04] – Henrik Mau | resources:tools-software:linuxdsp:docs:quickstartguide:sharc-alsa-example [14 Sep 2023 10:12] (current) – Vasileios Bimpikas |
---|
| <note warning>These pages are not updated anymore. Documentation has been moved to [[https://github.com/analogdevicesinc/lnxdsp-adi-meta/wiki|https://github.com/analogdevicesinc/lnxdsp-adi-meta/wiki]]</note> |
| |
| |
===== SHARC-ALSA Example ===== | ===== SHARC-ALSA Example ===== |
| <note>SHARC-ALSA is currently supported only on SC598</note> |
| |
<note important>In order to run the SHARC-ALSA example it is necessary to follow the instructions on [[resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc594_beta|Yocto Linux Quickstart Guide for ADSP-SC594 Development Branch]] and enable the SHARC-ALSA example as part of the build.</note> | <note important>For releases **prior** to [[resources:tools-software:linuxdsp:releaselandingpages:3.0.0|Linux for ADSP-SC5xx Processors 3.0.0]], follow [[:resources:tools-software:linuxdsp:docs:quickstartguide:sharc-alsa-example_legacy|SHARC-ALSA example (legacy)]]</note> |
| |
| <note>SHARC-ALSA is **not** enabled by default when following the Quickstart guides within [[resources:tools-software:linuxdsp:releaselandingpages:3.0.0|Linux for ADSP-SC5xx Processors 3.0.0]]. You need to change the final line in the ''conf/local.conf'' file from ''DISTRO_FEATURES:append = " linux_only_audio"'' to ''DISTRO_FEATURES:append = " adi_sharc_alsa_audio"'' before building the image. |
| </note> |
| |
SHARC-ALSA is a framework designed to make a SHARC appear as an audio device in [[https://alsa-project.org/wiki/Main_Page|ALSA]]. It uses [[https://www.kernel.org/doc/html/latest/staging/rpmsg.html|RPMsg]] for the communication between the ARM Core and the SHARC Core. When playing audio through ALSA the audio samples are transferred to the SHARC where additional processing can take place before the audio is played. | SHARC-ALSA is a framework designed to make a SHARC appear as an audio device in [[https://alsa-project.org/wiki/Main_Page|ALSA]]. It uses [[https://www.kernel.org/doc/html/latest/staging/rpmsg.html|RPMsg]] for the communication between the ARM Core and the SHARC Core. When playing audio through ALSA the audio samples are transferred to the SHARC where additional processing can take place before the audio is played. |
| |
| ==== SHARC-ALSA modes ==== |
| |
| There are 2 modes for SHARC-ALSA, and they differ in how the SHARCs are programmed. The mode is set in the ''conf/local.conf'' file, when building the Linux image. E.g. : ''DISTRO_FEATURES:append = " adi_sharc_alsa_audio"'' |
| |
| |
| \\ |
| == adi_sharc_alsa_audio == |
| Audio playback handled through SHARC firmware, no codec control (volume, etc) from Linux. Remoteproc is used to load the SHARC LDR firmware files. |
| |
| \\ |
| == adi_sharc_alsa_audio_uboot == |
| Audio playback handled through SHARC firmware, no codec control (volume, etc) from Linux. Remoteproc is //not// used to load the SHARC LDR firmware file. |
| |
| |
\\ | \\ |
==== Programming the SHARC ==== | ==== Programming the SHARC ==== |
An example SHARC image providing 2-channel playback is present in the /lib/firmware folder on the target. The SHARC can be programmed with this image using the sysfs interface to remoteproc as shown below: | |
| |
<code> | === Using Linux (remoteproc) === |
# echo 2Channel-SC594.ldr > /sys/class/remoteproc/remoteproc0/firmware | == adi_sharc_alsa_audio == |
# echo start > /sys/class/remoteproc/remoteproc0/state | An example SHARC image is present in the ''/lib/firmware'' directory on the target. The SHARC can be programmed with this image using the Linux shell. The SHARCs are running already when Linux has booted, so you can stop them, reload the example image or your own one, and start them again |
| <code bash> |
| $ cd /lib/firmware |
| |
| $ echo stop > /sys/class/remoteproc/remoteproc0/state |
| ADI Reset Control Unit 3108b000.rcu: Timeout waiting for remote core 1 to IDLE! |
| remoteproc remoteproc0: stopped remote processor core1-rproc |
| |
| $ echo icap-sharc-alsa_Core1.ldr > /sys/class/remoteproc/remoteproc0/firmware |
| |
| $ echo start > /sys/class/remoteproc/remoteproc0/state |
| remoteproc remoteproc0: powering up core1-rproc |
| remoteproc remoteproc0: Booting fw image adi_adsp_core1_fw.ldr, size 132860 |
| adi_remoteproc 28240000.core1-rproc: Core1 rpmsg init timeout, probably not supported. |
| virtio_rpmsg_bus virtio0: rpmsg host is online |
| remoteproc0#vdev0buffer: registered virtio0 (type 7) |
| remoteproc remoteproc0: remote processor core1-rproc is now up |
</code> | </code> |
| |
When executing the "echo start" command you will notice the LEDs on the SOMCRR-EZKIT flashing and then settle on LED7 remaining on. This indicates that the image on the SHARC is running. | When executing the ''echo start'' command you will notice the LEDs on the SOMCRR-EZKIT flashing and then settle on LED7 remaining on. This indicates that the image on the SHARC is running. |
| |
| \\ |
| |
| === Using U-Boot === |
| == adi_sharc_alsa_audio_uboot == |
| An example SHARC image is present in the /lib/firmware folder on the target. The SHARC can be programmed with this image via U-Boot. You need to store ''icap-sharc-alsa_Core1.ldr'' & ''icap-sharc-alsa_Core2.ldr'' (or your own image/images) in the TFTP server used throughout the booting process in the [[resources:tools-software:linuxdsp:releaselandingpages:3.0.0|Linux for ADSP-SC5xx Processors 3.0.0 (develop)]]. With these stored in the TFTP server, you need to input the following at the U-Boot prompt |
| |
| <code bash> |
| => rproc init |
| => tftp ${loadaddr} icap-sharc-alsa_Core1.ldr |
| => rproc load 0 ${loadaddr} ${filesize} |
| Load Remote Processor 0 with data@addr=0x96000000 132860 bytes: Success! |
| => tftp ${loadaddr} icap-sharc-alsa_Core2.ldr |
| => rproc load 1 ${loadaddr} ${filesize} |
| Load Remote Processor 1 with data@addr=0x96000000 79892 bytes: Success! |
| => rproc start 1 |
| => rproc start 0 |
| </code> |
| |
| You can now proceed to booting Linux as per usual. The SHARCs will be programmed and running. |
| |
\\ | \\ |
==== Playing Audio ==== | ==== Playing Audio ==== |
The audio from the SHARC is routed to DAC1/2. Connect a set of speakers to J17 also labelled as DAC1/2. | <note>The audio from the SHARC is routed to DAC1/2. Connect a set of speakers to J17 also labelled as DAC1/2.</note> |
Play back the audio sample file stored in /usr/share/sounds/alsa/ | {{:resources:tools-software:linuxdsp:docs:quickstartguide:adsp-sc594-som-ezkit-alsa-example.jpg?400|}} |
| |
| Play back the audio sample file stored in ''/usr/share/sounds/alsa/'' |
| |
<code> | <code bash> |
# aplay /usr/share/sounds/alsa/2Ch_L440_R200_48kHz_16bit_6s.wav | $ aplay /usr/share/sounds/alsa/2Ch_L440_R200_48kHz_16bit_6s.wav |
</code> | </code> |
| |
\\ | \\ |
=== Adding a Tone to a Channel === | === Adding a Tone to a Channel === |
The SHARC can be instructed to add a tone to the audio played using aplay. This is done through a command interface which also uses RPMsg for passing on the instructions to the SHARC Core. A helper tool for simplifying this is installed on the target. The tool creates a character device which will accept a channel number and a frequency to be added to the audio as strings allowing for simple interaction from the command line. | The SHARC can be instructed to add a tone to the audio played using aplay. This is done through a command interface which also uses RPMsg for passing on the instructions to the SHARC Core. A helper tool for simplifying this is installed on the target. The tool creates a character device which will accept a channel number and a frequency to be added to the audio as strings allowing for simple interaction from the command line. |
| |
<code> | <code bash> |
# rpmsg-bind-chardev -d virtio0.sharc-audioweaver.-1.201 -a 60 | $ rpmsg-bind-chardev -d virtio0.sharc-audioweaver.-1.201 -a 60 |
</code> | </code> |
| |
Once the binding has been created a character device /dev/rpmsg0 is available and will accept commands with the syntax <channel> <frequency>. To add a 800Hz tone to channel 0 (Left) enter the following at the command line: | Once the binding has been created a character device /dev/rpmsg0 is available and will accept commands with the syntax <channel> <frequency>. To add a 800Hz tone to channel 0 (Left) enter the following at the command line: |
<code> | <code bash> |
# echo 0 800.0 > /dev/rpmsg0 | $ echo 0 800.0 > /dev/rpmsg0 |
</code> | </code> |
| |
Similarly to add a 500Hz tone to channel 1 (Right) enter the following command: | Similarly to add a 500Hz tone to channel 1 (Right) enter the following command: |
<code> | <code bash> |
# echo 1 500.0 > /dev/rpmsg0 | $ echo 1 500.0 > /dev/rpmsg0 |
</code> | </code> |
| |
When running aplay again you will hear a dual tone frequency on both channels. Left channel will contain 440Hz + 800Hz whereas the right channel will contain 200Hz + 500Hz. | When running aplay again you will hear a dual tone frequency on both channels. The left channel will contain 440Hz + 800Hz whereas the right channel will contain 200Hz + 500Hz. |
<code> | <code bash> |
# aplay /usr/share/sounds/alsa/2Ch_L440_R200_48kHz_16bit_6s.wav | $ aplay /usr/share/sounds/alsa/2Ch_L440_R200_48kHz_16bit_6s.wav |
</code> | </code> |
| |