This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:linuxdsp:docs:quickstartguide:quickstart_sc589_2_2_0 [19 Jan 2023 11:24] – Fixed wrong arguments to repo init Vasileios Bimpikas | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ===== Yocto Linux 2.2.0 Quickstart Guide for ADSP-SC589 (EZKIT & MINI) ===== | ||
+ | <note important> | ||
+ | <note important> | ||
+ | For instructions for other processors and development boards please refer to [[resources: | ||
+ | ===== Setting Up Your Host PC ===== | ||
+ | The build system is currently supported on host PCs running Ubuntu 20.04 LTS 64-bit. | ||
+ | |||
+ | \\ | ||
+ | ==== Installing Required Packages ==== | ||
+ | |||
+ | In order to build and deploy Linux to your ADSP-SC589-EZKIT or ADSP-SC589-MINI development board you will need to install the following packages on your host PC. | ||
+ | |||
+ | < | ||
+ | $ sudo apt-get update | ||
+ | $ sudo apt-get install -y gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm u-boot-tools openssl curl tftpd-hpa python | ||
+ | </ | ||
+ | |||
+ | |||
+ | \\ | ||
+ | ==== Installing CrossCore Embedded Studio ==== | ||
+ | CrossCore Embedded Studio contains OpenOCD which is used to transfer U-Boot into RAM for the first initial boot of the device. | ||
+ | |||
+ | < | ||
+ | $ wget http:// | ||
+ | $ sudo dpkg -i ./ | ||
+ | $ sudo apt install lib32z1 | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ==== Configuring TFTP Service==== | ||
+ | A TFTP server on the host is used to transfer images to the development board. | ||
+ | Install and configure. | ||
+ | |||
+ | < | ||
+ | $ sudo vi / | ||
+ | |||
+ | #Replace the existing file with the following | ||
+ | TFTP_USERNAME=" | ||
+ | TFTP_DIRECTORY="/ | ||
+ | TFTP_ADDRESS=" | ||
+ | TFTP_OPTIONS=" | ||
+ | #End of File | ||
+ | |||
+ | $ sudo mkdir /tftpboot | ||
+ | $ sudo chmod 777 /tftpboot | ||
+ | $ sudo service tftpd-hpa restart | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ==== Configure Minicom ==== | ||
+ | In order to communicate with the U-Boot bootloader, a UART connection must be made between the host PC and the development board. It is recommended that you use minicom to do this. Minicom must be configured to connect to U-Boot correctly. | ||
+ | |||
+ | On the host PC open a terminal and execute the following commands: | ||
+ | |||
+ | < | ||
+ | $ sudo apt-get install -y minicom | ||
+ | $ sudo minicom -s | ||
+ | |||
+ | +-----[configuration]------+ | ||
+ | | Filenames and paths | | ||
+ | | File transfer protocols | ||
+ | | Serial port setup | | ||
+ | | Modem and dialing | ||
+ | | Screen and keyboard | ||
+ | | Save setup as dfl | | ||
+ | | Save setup as.. | | ||
+ | | Exit | | ||
+ | | Exit from Minicom | ||
+ | +--------------------------+ | ||
+ | |||
+ | |||
+ | # Select Serial port setup | ||
+ | Set Serial Device to / | ||
+ | Set Bps/ | ||
+ | Set Hardware Flow Control to No | ||
+ | |||
+ | Close the Serial port setup option by press Esc | ||
+ | | ||
+ | | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ==== Installing the Sources ==== | ||
+ | The example is fully contained in the Analog Devices Yocto Linux github repositories. | ||
+ | |||
+ | To install the sources: | ||
+ | |||
+ | < | ||
+ | $ mkdir ~/griffin | ||
+ | $ cd ~/griffin | ||
+ | $ mkdir bin | ||
+ | $ curl http:// | ||
+ | $ chmod a+x ./bin/repo | ||
+ | $ ./bin/repo init \ | ||
+ | -u https:// | ||
+ | -b develop/ | ||
+ | -m develop-yocto-2.2.0.xml | ||
+ | $ ./bin/repo sync | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ===== Building the Image ===== | ||
+ | ==== Preparing the buildtool ==== | ||
+ | Yocto requires the environment to be configured before building is possible. A setup-environment script in the griffin folder contains all the required environment settings for your build target. | ||
+ | Source the setup script for your board: | ||
+ | < | ||
+ | $ source setup-environment -m adsp-sc589-ezkit | ||
+ | </ | ||
+ | or | ||
+ | < | ||
+ | $ source setup-environment -m adsp-sc589-mini | ||
+ | </ | ||
+ | |||
+ | Sourcing the script will configure your build environment and create a build folder along with a local build configuration file. See the Yocto Manual for further details. | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | \\ | ||
+ | ==== Building the example ==== | ||
+ | You can build three different versions of the root file system; minimal, ramdisk and full. | ||
+ | To build the example images invoke bitbake from within the build directory created previously. | ||
+ | |||
+ | < | ||
+ | $ bitbake adsp-sc5xx-minimal | ||
+ | $ bitbake adsp-sc5xx-ramdisk | ||
+ | $ bitbake adsp-sc5xx-full | ||
+ | </ | ||
+ | |||
+ | When the build completes you will see a warning that the ELF binary has relocations in .text. It is OK to ignore this warning | ||
+ | |||
+ | |||
+ | Copy the U-Boot binary files to the tftp directory: | ||
+ | |||
+ | < | ||
+ | $ cp tmp/ | ||
+ | $ cp tmp/ | ||
+ | $ cp tmp/ | ||
+ | </ | ||
+ | or | ||
+ | < | ||
+ | $ cp tmp/ | ||
+ | $ cp tmp/ | ||
+ | $ cp tmp/ | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ==== Running U-Boot on the Board for the first time==== | ||
+ | |||
+ | Before installing the software on to the development board, ensure that the following cables are connected: | ||
+ | * Board connected to network via ethernet cable using J14 connector. | ||
+ | * Board connected to host PC using USB micro cable, connected to USB/ | ||
+ | * Board connected to the ICE 1000 or ICE 2000 via the DEBUG port on the board | ||
+ | * ICE is also connected to host PC via USB mini cable | ||
+ | |||
+ | {{: | ||
+ | {{: | ||
+ | |||
+ | * **// | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The console output from U-Boot and later on Linux will appear on the USB serial port configured in minicom earlier so open up minicom. | ||
+ | ;'' | ||
+ | :< | ||
+ | |||
+ | In a separate console launch OpenOCD and connect to the development board | ||
+ | |||
+ | |||
+ | ;'' | ||
+ | :< | ||
+ | $ cd / | ||
+ | $ sudo / | ||
+ | Where < | ||
+ | When successful you should see a message similar to the console output below | ||
+ | < | ||
+ | Open On-Chip Debugger (Analog Devices CCES 2.10.0 OpenOCD 0.9.0-ga8d0a22) 0.9.0 | ||
+ | Licensed under GNU GPL v2 | ||
+ | Report bugs to < | ||
+ | adapter speed: 1000 kHz | ||
+ | Info : transports supported by the debug adapter: " | ||
+ | Info : auto-select transport " | ||
+ | halt and restart using CTI | ||
+ | trst_only separate trst_push_pull | ||
+ | Info : ICE-1000 firmware version is 1.0.2 | ||
+ | Info : clock speed 1000 kHz | ||
+ | Info : JTAG tap: adspsc58x.adjc tap/device found: 0x228080cb (mfg: 0x065, part: 0x2808, ver: 0x2) | ||
+ | Info : JTAG tap: adspsc58x.dap enabled | ||
+ | Info : adspsc58x.dap: | ||
+ | Info : adspsc58x.dap: | ||
+ | </ | ||
+ | |||
+ | In a third console window launch GDB and type '' | ||
+ | ;'' | ||
+ | : < | ||
+ | $ cd /tftpboot | ||
+ | $ / | ||
+ | ... | ||
+ | (gdb) target extended-remote :3333 | ||
+ | Remote debugging using :3333 | ||
+ | 0x00004884 in ?? () | ||
+ | (gdb) load init-sc589-ezkit.elf | ||
+ | Loading section .text, size 0xa70 lma 0x20080000 | ||
+ | Start address 0x20080028, load size 2672 | ||
+ | Transfer rate: 25 KB/sec, 2672 bytes/ | ||
+ | (gdb) c | ||
+ | Continuing. | ||
+ | ^C | ||
+ | Program received signal SIGINT, Interrupt. | ||
+ | 0x20080024 in ?? () | ||
+ | </ | ||
+ | |||
+ | ;'' | ||
+ | : < | ||
+ | $ cd /tftpboot | ||
+ | $ / | ||
+ | ... | ||
+ | (gdb) target remote :3333 | ||
+ | Remote debugging using :3333 | ||
+ | 0x00004884 in ?? () | ||
+ | (gdb) load init-sc589-mini.elf | ||
+ | Loading section .text, size 0xa70 lma 0x20080000 | ||
+ | Start address 0x20080028, load size 2672 | ||
+ | Transfer rate: 25 KB/sec, 2672 bytes/ | ||
+ | (gdb) c | ||
+ | Continuing. | ||
+ | ^C | ||
+ | Program received signal SIGINT, Interrupt. | ||
+ | 0x20080024 in ?? () | ||
+ | </ | ||
+ | |||
+ | |||
+ | Now, load U-Boot into RAM. | ||
+ | |||
+ | ;'' | ||
+ | : | ||
+ | < | ||
+ | (gdb) load | ||
+ | Loading section .text, size 0x3a8 lma 0x89200000 | ||
+ | Loading section .efi_runtime, | ||
+ | Loading section .text_rest, size 0x4dd10 lma 0x892011e0 | ||
+ | Loading section .rodata, size 0xfbe0 lma 0x8924eef0 | ||
+ | Loading section .hash, size 0x18 lma 0x8925ead0 | ||
+ | Loading section .dtb.init.rodata, | ||
+ | Loading section .data, size 0x3468 lma 0x8925ee50 | ||
+ | Loading section .got.plt, size 0xc lma 0x892622b8 | ||
+ | Loading section .u_boot_list, | ||
+ | Loading section .efi_runtime_rel, | ||
+ | Loading section .rel.dyn, size 0xb180 lma 0x89263214 | ||
+ | Loading section .dynsym, size 0x30 lma 0x8926e394 | ||
+ | Loading section .dynstr, size 0x1 lma 0x8926e3c4 | ||
+ | Loading section .dynamic, size 0x90 lma 0x8926e3c8 | ||
+ | Loading section .gnu.hash, size 0x18 lma 0x8926e458 | ||
+ | Start address 0x89200000, load size 451677 | ||
+ | Transfer rate: 31 KB/sec, 11581 bytes/ | ||
+ | (gdb) c | ||
+ | Continuing. | ||
+ | </ | ||
+ | |||
+ | ;'' | ||
+ | : | ||
+ | < | ||
+ | (gdb) load | ||
+ | Loading section .text, size 0x3a8 lma 0xc2200000 | ||
+ | Loading section .efi_runtime, | ||
+ | Loading section .text_rest, size 0x4f4a0 lma 0xc22011e0 | ||
+ | Loading section .rodata, size 0xff43 lma 0xc2250680 | ||
+ | Loading section .hash, size 0x18 lma 0xc22605c4 | ||
+ | Loading section .dtb.init.rodata, | ||
+ | Loading section .data, size 0x3390 lma 0xc2260940 | ||
+ | Loading section .got.plt, size 0xc lma 0xc2263cd0 | ||
+ | Loading section .u_boot_list, | ||
+ | Loading section .efi_runtime_rel, | ||
+ | Loading section .rel.dyn, size 0xb218 lma 0xc2264c2c | ||
+ | Loading section .dynsym, size 0x30 lma 0xc226fe44 | ||
+ | Loading section .dynstr, size 0x1 lma 0xc226fe74 | ||
+ | Loading section .dynamic, size 0x90 lma 0xc226fe78 | ||
+ | Loading section .gnu.hash, size 0x18 lma 0xc226ff08 | ||
+ | Start address 0xc2200000, load size 458512 | ||
+ | Transfer rate: 30 KB/sec, 11462 bytes/ | ||
+ | (gdb) c | ||
+ | Continuing. | ||
+ | </ | ||
+ | |||
+ | At this point U-Boot will now be running in RAM on your target board. You should see U-Boot booting in the minicom console (Terminal 1). Press a key to interrupt the boot process before the countdown terminates: | ||
+ | ;'' | ||
+ | : < | ||
+ | U-Boot 2020.10 (Aug 23 2022 - 13:09:23 +0000) | ||
+ | |||
+ | CPU: ADSP ADSP-SC589-0.1 (Detected Rev: 1.1) (spi flash boot) | ||
+ | VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 450 MHz | ||
+ | OCLK: 150 MHz | ||
+ | Model: ADI sc589-ezkit | ||
+ | I2C: ready | ||
+ | DRAM: 224 MiB | ||
+ | MMC: SC5XX SDH: 0 | ||
+ | Loading Environment from SPIFlash... | ||
+ | SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB | ||
+ | *** Warning - bad CRC, using default environment | ||
+ | |||
+ | In: serial@0x31003000 | ||
+ | Out: | ||
+ | Err: | ||
+ | SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB | ||
+ | other init | ||
+ | Net: | ||
+ | Hit any key to stop autoboot: | ||
+ | => | ||
+ | </ | ||
+ | |||
+ | ;'' | ||
+ | : < | ||
+ | U-Boot 2020.10 (Aug 23 2022 - 13:09:23 +0000) | ||
+ | |||
+ | CPU: ADSP ADSP-SC589-0.1 (Detected Rev: 1.1) (spi flash boot) | ||
+ | VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 450 MHz | ||
+ | OCLK: 150 MHz | ||
+ | Model: ADI sc589-mini | ||
+ | I2C: ready | ||
+ | DRAM: 224 MiB | ||
+ | MMC: SC5XX SDH: 0 | ||
+ | Loading Environment from SPIFlash... | ||
+ | SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB | ||
+ | *** Warning - bad CRC, using default environment | ||
+ | |||
+ | In: serial@0x31003000 | ||
+ | Out: | ||
+ | Err: | ||
+ | other init | ||
+ | Net: | ||
+ | Hit any key to stop autoboot: | ||
+ | => | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | == Flash U-Boot to SPI Flash == | ||
+ | |||
+ | \\ | ||
+ | In the U-Boot console, set the IP address of the Host Linux PC that hosts the U-Boot loader file ('' | ||
+ | ;'' | ||
+ | : | ||
+ | < | ||
+ | => setenv serverip < | ||
+ | </ | ||
+ | |||
+ | < | ||
+ | |||
+ | If your network **supports** DHCP, run: | ||
+ | < | ||
+ | => dhcp | ||
+ | </ | ||
+ | |||
+ | If your network **does NOT support** DHCP, run: | ||
+ | < | ||
+ | => set ipaddr < | ||
+ | </ | ||
+ | |||
+ | Where ''< | ||
+ | |||
+ | Next, run the U-Boot update command to copy the U-Boot loader file from the host PC to the target board, and write it into flash: | ||
+ | < | ||
+ | => run update | ||
+ | </ | ||
+ | |||
+ | You will see an output similar to the one below: | ||
+ | < | ||
+ | => run update | ||
+ | Speed: 1000, full duplex | ||
+ | Using dwmac.3100c000 device | ||
+ | TFTP from server 192.168.1.223; | ||
+ | Filename ' | ||
+ | Load address: 0xc2000000 | ||
+ | Loading: ################################ | ||
+ | 3.8 MiB/s | ||
+ | done | ||
+ | Bytes transferred = 459144 (70188 hex) | ||
+ | SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB | ||
+ | SF: 524288 bytes @ 0x0 Erased: OK | ||
+ | device 0 offset 0x0, size 0x70188 | ||
+ | SF: 459144 bytes @ 0x0 Written: OK | ||
+ | => | ||
+ | </ | ||
+ | |||
+ | At this point the U-Boot binary is stored in flash. You can now disconnect the ICE-1000 or ICE-2000 from the development board and make sure to switch the BMODE to position 1. You will only need to reconnect this if your board fails to boot and you need to re-follow these instructions. | ||
+ | \\ | ||
+ | |||
+ | ===== Booting Linux ===== | ||
+ | ==== Booting Linux Using SD Card ==== | ||
+ | === Formatting the SD Card === | ||
+ | In order to use an SD Card with Linux we need to prepare it by formatting it in the correct format. | ||
+ | This section of instructions requires you to correctly identify the SD Card and format the card. If you select the wrong drive you may cause irreversible damage to you Host PC. | ||
+ | To format the SD Card, follow the commands below. The example code in this section assumes that the SD Card device is reported to be /dev/sdb. Ensure that you change these commands to use your device. | ||
+ | < | ||
+ | $ sudo fdisk /dev/sdb | ||
+ | /* Create primary partition 1, 256M size*/ | ||
+ | Command (m for help): n | ||
+ | Select (default p): p | ||
+ | Partition number (1-4, default 1): 1 | ||
+ | First sector (2048-3887103, | ||
+ | Last sector, +sectors or +size{K, | ||
+ | |||
+ | /* Save partition */ | ||
+ | Command (m for help): w | ||
+ | </ | ||
+ | |||
+ | Format the SD card to EXT filesystem | ||
+ | < | ||
+ | $ sudo mkfs.ext2 /dev/sdb1 | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | === Writing the kernel and file system to the SD Card === | ||
+ | Next, we need to copy the Linux file system and kernel image to the SD Card. We install this on to the SD Card by mounting the file system on to the local Host PC and copying the contents on to the SD Card. To allow the choice of booting using ramboot and sdcard boot we copy the ramboot image to the SD card as well as extract the minimal image to the SD card. | ||
+ | < | ||
+ | $ mkdir ~/mnt | ||
+ | $ sudo mount -t ext2 /dev/sdb1 ~/mnt | ||
+ | $ sudo mkdir ~/mnt/boot | ||
+ | $ sudo cp tmp/ | ||
+ | $ sudo cp tmp/ | ||
+ | $ sudo cp tmp/ | ||
+ | $ sudo tar -xf tmp/ | ||
+ | $ sudo umount ~/mnt | ||
+ | </ | ||
+ | or | ||
+ | < | ||
+ | $ mkdir ~/mnt | ||
+ | $ sudo mount -t ext2 /dev/sdb1 ~/mnt | ||
+ | $ sudo mkdir ~/mnt/boot | ||
+ | $ sudo cp tmp/ | ||
+ | $ sudo cp tmp/ | ||
+ | $ sudo cp tmp/ | ||
+ | $ sudo tar -xf tmp/ | ||
+ | $ sudo umount ~/mnt | ||
+ | </ | ||
+ | |||
+ | The file system and kernel image are now installed on to the SD Card. The SD Card can now be safely removed from the Host PC. | ||
+ | |||
+ | \\ | ||
+ | === Booting Linux from the SD card === | ||
+ | Insert the SD card to target board, and reset the board and enter into U-Boot | ||
+ | < | ||
+ | => run sdcardboot | ||
+ | or | ||
+ | => run ramboot_emmc | ||
+ | </ | ||
+ | |||
+ | The linux kernel will then boot up using the file system stored in SD card. | ||
+ | |||
+ | \\ | ||
+ | ==== Booting Linux Using TFTP ==== | ||
+ | In order to boot Linux, the TFTP server should be setup as [[resources/ | ||
+ | |||
+ | < | ||
+ | $ cp tmp/ | ||
+ | </ | ||
+ | or | ||
+ | < | ||
+ | $ cp tmp/ | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | === RAM Boot === | ||
+ | For RAM boot we need to copy the image containing filesystem to the /tftpboot directory. | ||
+ | < | ||
+ | $ cp tmp/ | ||
+ | </ | ||
+ | or | ||
+ | < | ||
+ | $ cp tmp/ | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | === NFS Boot === | ||
+ | For NFS boot we use the Network File System which is stored in local Ubuntu Host. This is suggested when you do application development. To setup the NFS server: | ||
+ | < | ||
+ | $ sudo apt-get install nfs-kernel-server | ||
+ | $ sudo vi / | ||
+ | |||
+ | #Add following commands | ||
+ | /romfs *(rw, | ||
+ | |||
+ | $ sudo mkdir /romfs/ | ||
+ | $ sudo chmod 777 /romfs/ | ||
+ | $ sudo service nfs-kernel-server start | ||
+ | </ | ||
+ | The file system is then copied to /romfs. \\ | ||
+ | |||
+ | If you are using the ADSP-SC589-EZKIT with the full image (you ran ' | ||
+ | < | ||
+ | $ sudo tar -xf tmp/ | ||
+ | </ | ||
+ | Or if you are using the ADSP-SC589-EZKIT with the minimal image (you ran ' | ||
+ | < | ||
+ | $ sudo tar -xf tmp/ | ||
+ | </ | ||
+ | Or if you are using the ADSP-SC589-MINI with the full image (you ran ' | ||
+ | < | ||
+ | $ sudo tar -xf tmp/ | ||
+ | </ | ||
+ | Or if you are using the ADSP-SC589-MINI with the minimal image (you ran ' | ||
+ | < | ||
+ | $ sudo tar -xf tmp/ | ||
+ | </ | ||
+ | \\ | ||
+ | === Booting into Linux from TFTP === | ||
+ | Next, on the target, from u-boot, run one of the following command: | ||
+ | < | ||
+ | => run ramboot | ||
+ | or | ||
+ | => run nfsboot | ||
+ | ...... | ||
+ | ...... | ||
+ | | ||
+ | [ OK ] Started Update UTMP about System Runlevel Changes. | ||
+ | |||
+ | |||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | |||
+ | Analog Devices Yocto Distribution | ||
+ | | ||
+ | www.yoctoproject.org | ||
+ | |||
+ | adsp-sc589-ezkit login: root | ||
+ | Password: adi | ||
+ | root@adsp-sc589-ezkit: | ||
+ | </ | ||
+ | |||
+ | The default username is **root** and the password is **adi**. | ||
+ | |||
+ | \\ | ||
+ | ==== Building the SDK ==== | ||
+ | To build the SDK follow the instructions here [[: |