This is an old revision of the document!
This documentation guides users how to develop Yocto Linux Products on ADI SC5XX platforms with developers' own repositories.
$ sudo apt-get update $ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm u-boot-tools $ sudo apt-get install repo
$ mkdir ~/yocto $ repo init -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git
$ cd ~/yocto/.repo/manifests/
Aplly below patches into the lnxdsp-repo-manifest
diff --git a/default.xml b/default.xml index 244bf04..45abdf8 100644 --- a/default.xml +++ b/default.xml @@ -5,12 +5,12 @@ <remote fetch="https://git.yoctoproject.org/git" name="yocto"/> <remote fetch="https://github.com/openembedded" name="oe"/> - <remote fetch="https://github.com/analogdevicesinc" name="adigithub"/> + <remote fetch="$YOUR_REPO_PATH" name="dte"/> <project remote="yocto" revision="50f33d3bfebcbfb1538d932fb487cfd789872026" name="poky" path="sources/poky"/> <!-- thud revision --> <project remote="oe" revision="4cd3a39f22a2712bfa8fc657d09fe2c7765a4005" name="meta-openembedded" path="sources/meta-openembedded"/> <!-- thud revision --> - <project remote="adigithub" revision="develop/yocto-1.0.0" name="lnxdsp-adi-meta" path="sources/meta-adi"/> - <project remote="adigithub" revision="develop/yocto-1.0.0" name="lnxdsp-scripts" path="sources"> + <project remote="dte" revision="develop/yocto-1.0.0" name="lnxdsp-adi-meta" path="sources/meta-adi"/> + <project remote="dte" revision="develop/yocto-1.0.0" name="lnxdsp-scripts" path="sources"> <linkfile dest="setup-environment" src="setup-environment"/> </project>>
$ repo sync
$ cd ~/yocto/sources/
Aplly below patches into your own build script, take adsp-sc589-ezkit as an example, the same patch should be applied into adsp-sc589-mini, adsp-sc584-ezkit, adsp-sc573-ezkit.
diff --git a/base/adsp-sc589-ezkit/local.conf b/base/adsp-sc589-ezkit/local.conf index 260a16b..b3c69f1 100644 --- a/base/adsp-sc589-ezkit/local.conf +++ b/base/adsp-sc589-ezkit/local.conf @@ -21,6 +21,11 @@ # This sets the default machine to be adsp-sc589-ezkit if no other machine is selected: MACHINE ?= "adsp-sc589-ezkit" +UBOOT_GIT_URI ?= "git://$YOUR_REPO_PATH/u-boot.git" +UBOOT_BRANCH ?= "develop/yocto-1.0.0" +KERNEL_GIT_URI ?= "git://$YOUR_REPO_PATH/lnxdsp-linux.git" +KERNEL_BRANCH ?= "develop/yocto-1.0.0" + # # Where to place downloads #
Then you can start your development based on your own repos.
$ cd ~/yocto/ $ source setup-environment -m adsp-sc589-ezkit Your build environment has been configured with: MACHINE=adsp-sc589-ezkit You can now run 'bitbake <target>' Some of common targets are: u-boot-adi linux-adi adsp-sc5xx-full adsp-sc5xx-minimal adsp-sc5xx-ramdisk $ bitbake ...