Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp [22 Sep 2020 11:11] – [Device tree configuration] Sunny Fengresources:tools-software:linuxdsp:docs:linux_yocto_distribution_and_applications:linuxptp [22 Sep 2020 11:14] (current) – [Device tree configuration] Sunny Feng
Line 48: Line 48:
 The timestamps that are the basis of PTP can be acquired with greater accuracy when they are captured by the ethernet PHY hardware. The PHY interface can support hardware timestamps, the default phy-mode is RGMII. The timestamps that are the basis of PTP can be acquired with greater accuracy when they are captured by the ethernet PHY hardware. The PHY interface can support hardware timestamps, the default phy-mode is RGMII.
  
-The phy-mode also can be changed to "rmii" in the device tree header in the linux kernel source arch/arm/boot/dts/sc589-ezkit.dts other board specific sc5xx.dts files. Run "//**bitbake linux-adi -c devshell**//" to enter into linux kernel source code.+The phy-mode also can be changed to "rmii" in the device tree header in the linux kernel source arch/arm/boot/dts/sc589-ezkit.dts and other board specific sc5xx.dts files. 
 <WRAP info> <WRAP info>
 ... : ellipsis, means other properties in EMAC0 node stay the same\\ ... : ellipsis, means other properties in EMAC0 node stay the same\\
resources/tools-software/linuxdsp/docs/linux_yocto_distribution_and_applications/linuxptp.1600765919.txt.gz · Last modified: 22 Sep 2020 11:11 by Sunny Feng