This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:start [27 Jul 2020 07:21] – cathy fang | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:start [27 Jan 2021 22:35] (current) – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | This document introduces usage of USB interface for SC5XX Linux. There are two different kinds of USB controller on SC5XX silicon, one supports [[https:// | + | This document introduces usage of USB interface for SC5XX Linux. There are two different kinds of USB controller on SC5XX silicon, one supports [[wp>USB_On-The-Go|OTG (On-The-Go) ]] for USB2.0, which is able to work as Host or Device dynamically according to the standard USB HNP protocol. Another support Host or Device only, dedicated hardware and software configurations should be made in advance to identify it is for Host or Device mode. |
** Example Usage Description ** | ** Example Usage Description ** |