Wireless_USB provides a approach for user to use the WIFI by adding a USB wireless dongle to the host (e.g. adsp-sc5xx board ) and the corresponding software configurations. This page describes how to use the USB Wireless (Wifi) feature on ADSP-sc5xx boards.
Using USB wireless Dongle in Linux:
Most of the USB Wireless Dongle need their own support drivers, and as the wireless driver in Linux kernel is to support the associated Wireless Network Chipset [e.g, Atheros/Qualcomm, Broadcom, Intel, Realtek]
no mater which the manufacturer (e.g. A-Link, Dell, D-Link, Philips, TP-link)
of the wireless card is, so we should make sure which chipset your device is using and enable/prepare the corresponding Linux drivers and Firmware first.
STEP1: Plug the USB Wireless Dongle into a Linux host PC and use the command “lsusb” to find the information of the device.
test@madara:~# lsusb Bus 002 Device 020: ID 2001:3306 D-Link Corp. DWL-G122 Wireless Adapter(rev.F1) [Realtek RTL8188SU] Bus 002 Device 019: ID 0cf3:7015 Atheros Communications, Inc. TP-Link TL-WN821N v3 / TL-WN822N v2 802.11n [Atheros AR7010+AR9287] Bus 002 Device 021: ID 0bda:818b Realtek Semiconductor Corp. RTL8192EU 802.11b/g/n WLAN Adapter
From the visit Linux-USB site: ID 2001:3306 is the number given to this chipset, The number before: indicates the manufacture ID and number after : indicates device ID.
STEP2: Query the Wireless Chipset corresponding supported driver and firmware from Google or other ways, here are some quick reference:
Now we can get the information of the chipset and it corresponding drivers and Firmware:
Realtek RTL8188SU
rtl8172u.ko
lib/firmware/rtlwifi/rtl8712u.bin
Atheros AR7010+AR9287
ath9k.ko
lib/firmware/ath9k_htc/htc_7010-1.4.0.fw
Realtek RTL8192EU 802.11b/g/n
RTL8xxxEU.ko
lib/firmware/rtlwifi/rtl8192eu_nic.bin
Connect the USB micro-A plug to A receptacle adaptor cable (found in the EZ-Board box) to the OTG port, below photo shows when it acts as Host and connected to a USB Wireless dongle device.
On the Yocto, Configure the linux-kernel as below to set the USB controller in Host only mode, and enable the USB wireless relevant supported operations.
Configure the USB drivers to host mod or (dual role mode)
Device Drivers ---> [*] USB support ---> <*> Support for Host-side USB [*] Enable USB persist by default <*> Inventra Highspeed Dual Role Controller MUSB Mode Selection (Dual role mode) ---> *** Platform Glue Layer *** <*> ADI *** MUSB DMA mode *** [N] Disable DMA (always use PIO) [*] Inventra
dual role mode need the g_serial and CDC module
Device Drivers ---> [*] USB support ---> <*> USB Gadget Support ---> <M> USB Gadget precomposed configurations <M> Serial Gadget (with CDC ACM and CDC OBEX support) <M> CDC Composite Device (Ethernet and ACM)
Configure the USB Wifi corresponding options
[*] Networking support ---> Networking options ---> [*] TCP/IP networking [*] IP: kernel level autoconfiguration [*] IP: DHCP support [*] IP: BOOTP support [*] IP: RARP support <*> The IPv6 protocol ---> [*] Wireless ---> <*> cfg80211 - wireless configuration API [*] cfg80211 wireless extensions compatibility <*> Generic IEEE 802.11 Networking Stack (mac80211) [*] Minstrel [*] Minstrel 802.11n support [*] Minstrel 802.11ac support
Enable the Wireless Chipset supported Drivers
For the ID 2001:3306
chipset Realtek RTL8188SU
Device Drivers ---> [*] Network device support ---> [*] Wireless LAN ---> [*] Realtek devices [*] Staging drivers ---> <*> RealTek RTL8712U (RTL8192SU) Wireless LAN NIC driver
For the ID 0cf3:7015
chipset: Atheros AltAR7010+AR9287
For the ID 0bda:818b
chipset rtl8188eu
Adding the corresponding Firmware
Standard Yocto layer provides a “sources/poky/meta/recipes-kernel/linux-firmware/linux-firmware_git.bb” for user to get some common firmware. please modify and add the below codes to sources/meta-adi/meta-adi-adsp-sc5xx/recipes-adi/images/adsp-sc5xx-full.bb
to enable the wpa-supplicant and wireless-tools tools and the chipset corresponding Firmware.
USB_WIFI = " \ wpa-supplicant \ wireless-tools \ linux-firmware-ath9k \ linux-firmware-rtl8192su \ " IMAGE_INSTALL += " \ ${USB_WIFI} \ "
Add the additional Firmware:
Reference:
sources/poky/meta/recipes-kernel/linux-firmware/linux-firmware_git.bb
Busy box configuration
bitbake busybox -c menuconfig
Coreutils ---> [*] mktemp (4 kb) Networking Utilities ---> [*] Enable IPv6 support [*] udhcpc [*] Verify that the offered address is free, using ARP ping [*] Do not pass malformed host and domain names --- Common options for DHCP applets (9) Maximum verbosity level (0..9) (80) DHCP options slack buffer size [*] Support RFC 3397 domain search options [*] Support 802.1Q VLAN parameters options (-R -b) ifup udhcpc command line options
Boot the generated Images and connect the USB Wireless Dongle to the target hardware board:
Step1. USB Wireless Dongle Detected
root@adsp-sc589-ezkit:~# modprobe g_serial (USB Dual mode) g_serial gadget: Gadget Serial v2.4 g_serial gadget: g_serial ready usb 1-1: new high-speed USB device number 2 using musb-hdrc r8712u: register rtl8712_netdev_ops to netdev_ops usb 1-1: r8712u: USB_SPEED_HIGH with 4 endpoints usb 1-1: r8712u: Boot from EFUSE: Autoload OK usb 1-1: r8712u: CustomerID = 0x0000 usb 1-1: r8712u: MAC Address from efuse = f0:7d:68:f1:3d:50 usb 1-1: r8712u: Loading firmware from "rtlwifi/rtl8712u.bin"
Step2. Enable the wlan0
and Scan the available wifi host
root@adsp-sc589-ezkit:~# ifconfig wlan0 up r8712u 1-1:1.0 wlan0: 1 RCR=0x153f00e r8712u 1-1:1.0 wlan0: 2 RCR=0x553f00e IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready root@adsp-sc589-ezkit:~# iwconfig wlan0 wlan0 unassociated Nickname:"rtl_wifi" Mode:Auto Access Point: Not-Associated Sensitivity:0/0 Retry:off RTS thr:off Fragment thr:off Encryption key:off Power Management:off Link Quality:0 Signal level:0 Noise level:0 Rx invalid nwid:0 Rx invalid crypt:0 Rx invalid frag:0 Tx excessive retries:0 Invalid misc:0 Missed beacon:0 root@adsp-sc589-ezkit:~# iwlist wlan0 scanning | grep ESSID ESSID:"ADIWLAN" ESSID:"ADIWLAN" ESSID:"iPhone" ESSID:"ADI-VISITOR" ESSID:"corpave" ESSID:"ChinaNet-7359" ESSID:"ADI-VISITOR"
Step3. Connect the WIFI Router host via wpa_supplicant tool
Configure the /etc/wpa_supplicant.conf to add the name
and password
of the target Router host as below:
ctrl_interface=/var/run/wpa_supplicant ctrl_interface_group=0 update_config=1 network={ key_mgmt=NONE } network={ ssid="corpave" # name psk="ADI12345" # password key_mgmt=WPA-EAP WPA-PSK IEEE8021X NONE # way of encryption priority=1 # priority } network={ ssid="iPhone" psk="12345678" key_mgmt=WPA-EAP WPA-PSK IEEE8021X NONE priority=2 scan_ssid=1 }
Run the wpa_supplicant -B -Dwext -iwlan0 -c/etc/wpa_supplicant.conf to create the wireless establishment
root@adsp-sc589-ezkit:~# wpa_supplicant -B -Dwext -iwlan0 -c/etc/wpa_supplicant.conf Successfully initialized wpa_supplicant rfkill: Cannot get wiphy information USHIPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready root@adsp-sc589-ezkit:~# iwconfig wlan0 wlan0 IEEE 802.11bgn ESSID:"corpave" Nickname:"rtl_wifi" Mode:Managed Frequency:2.437 GHz Access Point: 14:D6:4D:32:3B:EA Bit Rate:150 Mb/s Sensitivity:0/0 Retry:off RTS thr:off Fragment thr:off Encryption key:****-****-****-****-****-****-****-**** Security mode:open Power Management:off Link Quality=100/100 Signal level=100/100 Noise level=0/100 Rx invalid nwid:0 Rx invalid crypt:0 Rx invalid frag:0 Tx excessive retries:0 Invalid misc:0 Missed beacon:0
Step4. Dynamic IP acquisition with the udhcpc
and Verification the wifi connection
root@adsp-sc589-ezkit:~# udhcpc -i wlan0 udhcpc: started, v1.29.3 udhcpc: sending discover udhcpc: sending select for 192.168.0.104 udhcpc: lease of 192.168.0.104 obtained, lease time 86400 /etc/udhcpc.d/50default: Adding DNS 192.168.0.1 root@adsp-sc589-ezkit:~# ifconfig wlan0 wlan0 Link encap:Ethernet HWaddr F0:7D:68:F1:3D:50 inet addr:192.168.0.104 Bcast:192.168.0.255 Mask:255.255.255.0 inet6 addr: fe80::f27d:68ff:fef1:3d50/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:58 errors:0 dropped:53 overruns:0 frame:0 TX packets:34 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:16072 (15.6 KiB) TX bytes:8747 (8.5 KiB) root@adsp-sc589-ezkit:~# route Kernel IP routing table Destination Gateway Genmask Flags Metric Ref Use Iface default 10.99.24.1 0.0.0.0 UG 0 0 0 eth0 default sqe-l12.ad.anal 0.0.0.0 UG 10 0 0 wlan0 10.99.24.0 * 255.255.255.0 U 0 0 0 eth0 192.168.0.0 * 255.255.255.0 U 0 0 0 wlan0 root@adsp-sc589-ezkit:~# ping 192.168.0.1 PING 192.168.0.1 (192.168.0.1): 56 data bytes 64 bytes from 192.168.0.1: seq=0 ttl=64 time=1.088 ms 64 bytes from 192.168.0.1: seq=1 ttl=64 time=0.956 ms 64 bytes from 192.168.0.1: seq=2 ttl=64 time=0.938 ms 64 bytes from 192.168.0.1: seq=3 ttl=64 time=0.898 ms 64 bytes from 192.168.0.1: seq=4 ttl=64 time=0.909 ms ^C --- 192.168.0.1 ping statistics --- 5 packets transmitted, 5 packets received, 0% packet loss round-trip min/avg/max = 0.898/0.957/1.088 ms
Help of Command wpa_supplicant
Go TO USB Interface