This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_wifi [27 Jan 2021 22:35] – use wp> interwiki links Robin Getz | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_wifi [04 Feb 2021 03:17] – cathy fang | ||
---|---|---|---|
Line 154: | Line 154: | ||
Add the additional Firmware: | Add the additional Firmware: | ||
< | < | ||
- | If we can't find the target chipset supported firmware from the **//linux-firmware_git.bb//**, we should write our own .bb file to fetch the corresponding Firmware or just adding it manually. | + | If we can't find the target chipset supported firmware from the linux-firmware_git.bb, |
**1. Manually fetch Firmware** | **1. Manually fetch Firmware** |