This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_wifi [27 Jul 2020 08:33] – [Hardware Configuration] cathy fang | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:host_mode:usb_wifi [04 Feb 2021 03:19] – cathy fang | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== USB to Wireless Dongle (Wifi) Support | ====== USB to Wireless Dongle (Wifi) Support | ||
- | [[https:// | + | [[wp>Wireless_USB|Wireless_USB]] provides a approach for user to use the WIFI by adding a USB wireless dongle to the host (e.g. adsp-sc5xx board ) and the corresponding software configurations. This page describes how to use the USB Wireless (Wifi) feature on ADSP-sc5xx boards. |
**Using USB wireless Dongle in Linux:** | **Using USB wireless Dongle in Linux:** | ||
Line 40: | Line 40: | ||
Connect the USB micro-A plug to A receptacle adaptor cable (found in the EZ-Board box) to the OTG port, below photo shows when it acts as Host and connected to a USB Wireless dongle device. | Connect the USB micro-A plug to A receptacle adaptor cable (found in the EZ-Board box) to the OTG port, below photo shows when it acts as Host and connected to a USB Wireless dongle device. | ||
- | {{ : | + | {{ : |
Line 139: | Line 139: | ||
**Adding the corresponding Firmware** | **Adding the corresponding Firmware** | ||
- | Standard Yocto layer provides a "// | + | Standard Yocto layer provides a "// |
<code java> | <code java> | ||
USB_WIFI = " \ | USB_WIFI = " \ | ||
Line 154: | Line 154: | ||
Add the additional Firmware: | Add the additional Firmware: | ||
< | < | ||
- | If we can't find the target chipset supported firmware from the **//linux-firmware_git.bb//**, we should write our own .bb file to fetch the corresponding Firmware or just adding it manually. | + | If we can't find the target chipset supported firmware from the linux-firmware_git.bb, |
**1. Manually fetch Firmware** | **1. Manually fetch Firmware** |