This is an old revision of the document!
This page introduces the SRAM driver in ADI linux kernel for sc5xx ezkit boards. Users could allocate memory from specified sram pool defined in dts. sram_mmap driver in this page is an example for this. For how to enable the sram_mmap, please see the below sections.
vim conf/local.conf IMAGE_INSTALL_append = " sram-mmap-test"
bitbake linux-adi -c menuconfig Device Drivers ---> [*] Staging drivers ---> [N] icc driver ----
bitbake linux-adi -c menuconfig Device Drivers ---> Misc devices ---> [*] Generic on-chip SRAM driver [*] MMAP driver for sc5xx onchip SRAM [*] /proc/sraminfo support for sc5xx onchip SRAM
# sram_mmap /dev/sram_mmap sram mmaped 0x20084000 : 0x20085000 successfully! mmap pass. # cat /proc/sraminfo sram-icc@20080000: Total size: 4 KB Used sram: 0 KB Avail sram: 4 KB sram-reserved@20084000: Total size: 236 KB Used sram: 0 KB Avail sram: 236 KB
There are two main c file under the driver/sram/adi directory.
These 2 dts part will generate 2 memory pools from sram using “mmio-sram” driver.
sram0: sram-icc@20080000 { /* ICC SRAM 4KB */ compatible = "mmio-sram"; #address-cells = <1>; #size-cells = <1>; reg = <0x20080000 0x1000>; ranges = <0 0x20080000 0x1000>; }; sram1: sram-reserved@20084000 { compatible = "mmio-sram"; #address-cells = <1>; #size-cells = <1>; reg = <0x20084000 0x3B000>; ranges = <0 0x20084000 0x3B000>; };
If users want to allocate their own sram memory from sram pool in linux kernel, they should first
adi,sram = <&sram1>;
/* Get the sram pool from dts */ sram_pool = of_gen_pool_get(dev->of_node, "adi,sram", 0); if (!sram_pool) { pr_err("Unable to get sram pool!\n"); return -ENODEV; } /* Get the allocated virtual memory from sram pool */ vaddr = gen_pool_alloc(sram_pool, sram_size); if (!vaddr) { pr_warn("Faied to alloc sram from sram pool!\n"); } /* Remember: When you finish all the operations, free the allocated addr */ gen_pool_free(sram_pool, vaddr, sram_size);
Back to Kernel Features and Device Drivers for ADSP-SC5xx Yocto Linux