This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:remoteproc:remoteproc [07 Jul 2020 11:52] – Sunny Feng | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:remoteproc:remoteproc [03 Jan 2021 21:43] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 8: | Line 8: | ||
* ADSP-SC573 Ezkit or, | * ADSP-SC573 Ezkit or, | ||
* ADSP-SC589 MINI | * ADSP-SC589 MINI | ||
- | Nothing | + | No connections |
===== Software Configuration ===== | ===== Software Configuration ===== | ||
Line 30: | Line 30: | ||
+ | \\ | ||
===== How to Use the Remoteproc Framework ===== | ===== How to Use the Remoteproc Framework ===== | ||
==== Remote Processor Start ==== | ==== Remote Processor Start ==== | ||
Line 41: | Line 42: | ||
root@adsp-sc589-ezkit: | root@adsp-sc589-ezkit: | ||
</ | </ | ||
- | <WRAP info 100%>The blinky_Core1_sc589.ldr is a SHARC firmware | + | <WRAP info 100%>The blinky_Core1_sc589.ldr is one SHARC LED blinking application |
</ | </ | ||
Line 48: | Line 49: | ||
root@adsp-sc589-ezkit: | root@adsp-sc589-ezkit: | ||
</ | </ | ||
- | The LED would start blinky | + | The LED will start blinking |
==== Remote Processor Stop ==== | ==== Remote Processor Stop ==== | ||
- | Run the below command, | + | Run the below command, |
< | < | ||
root@adsp-sc589-ezkit: | root@adsp-sc589-ezkit: | ||
Line 57: | Line 58: | ||
==== Remote Processor Auto Boot ==== | ==== Remote Processor Auto Boot ==== | ||
- | ADI set a specified name called adi_adsp_core1_fw.ldr or adi_adsp_core2_fw.ldr to auto boot when kernel | + | ADI sets a specified name called adi_adsp_core1_fw.ldr or adi_adsp_core2_fw.ldr to auto boot when kernel |
If you want to auto boot the remote processor, rename your own ldr file to **adi_adsp_core1_fw.ldr** or **adi_adsp_core1_fw.ldr** and put it in **/ | If you want to auto boot the remote processor, rename your own ldr file to **adi_adsp_core1_fw.ldr** or **adi_adsp_core1_fw.ldr** and put it in **/ | ||
---- | ---- | ||
**Back to** [[resources: | **Back to** [[resources: |