This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mmc:mmc [17 Jul 2020 09:57] – [Formatting the SD Card] Sunny Feng | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mmc:mmc [17 Jul 2020 09:58] (current) – [Mount the MS-DOS file system on the SD Card] Sunny Feng | ||
---|---|---|---|
Line 109: | Line 109: | ||
</ | </ | ||
+ | \\ | ||
==== Mount the MS-DOS file system on the SD Card ==== | ==== Mount the MS-DOS file system on the SD Card ==== | ||
Line 191: | Line 192: | ||
</ | </ | ||
+ | \\ | ||
==== 2) Test Case 2: Bonnie++ on FAT32 ==== | ==== 2) Test Case 2: Bonnie++ on FAT32 ==== | ||
Input the following command on the target board console | Input the following command on the target board console |