This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:start [24 Jul 2020 11:07] – created Sunny Feng | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:start [14 Dec 2020 09:58] (current) – Sunny Feng | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Multi-Core | + | ====== Multi-Core |
+ | |||
+ | The Yocto Linux Product provides user space APIs that allow applications to easily communicate with the SHARC cores of the ADSP-SC5xx processor. | ||
+ | |||
+ | Communication is performed using the Multi-core Communications API (MCAPI) specification which defines an API and a semantics for communication and synchronization between processing cores in embedded systems. MCAPI is supported on the SHARC cores of the ADSP-SC5xx processors in both bare-metal and RTOS using CrossCore Embedded Studio. For more information about MCAPI, please refer to the MCAPI Specification document from MCAPI.org. | ||
ADSP-SC5xx is a series of products with multiple processor cores (two SHARC+ cores and an ARM® Cortex-A5 processor), this page provides some approaches to support the multi-core communication/ | ADSP-SC5xx is a series of products with multiple processor cores (two SHARC+ cores and an ARM® Cortex-A5 processor), this page provides some approaches to support the multi-core communication/ | ||
; **'' | ; **'' | ||
- | : [[resources: | + | : [[resources: |
+ | ; **'' | ||
: [[resources: | : [[resources: | ||
+ | : [[resources: | ||
+ | |||
; **'' | ; **'' | ||
- | : [[resources: | + | : [[resources: |
- | : Introduction of MCAPI examples | + | : [[resources: |
- | : [[resources: | + | : [[resources: |
- | ; **'' | + | |
- | : [[resources: | + | |
- | : SEC driver and multicore development | + | |
- | + | ||
| | ||
| |