This is an old revision of the document!
This document introduces two kind of core control solutions which support ADSP-SC573, SC584, SC589 EZ-Kits and SC589-MINI. One method is to control SHARC Cores with u-boot ICC command. Other way includes a kernel device driver and a command-line utility, for enabling and disabling the SHARC cores (Core 1 & 2) from the ARM core (Core 0), which have been added to the Yocto Linux distribution for ADSP-SC573, SC584, SC589 and SHARC AUDIO MODULE.
The slave SHARC core 0 and 1 in SC5xx silicon can be enabled and disabled in u-boot command console. In order to include this ICC command into u-boot, you need to select it in u-boot configuration.
$ bitbake u-boot-adi -c menuconfig ARM architecture ---> [*] ICC command to enable and disable slave cores
After saving the configuration in u-boot, rebuild the u-boot ldr image for sc5xx boards.
$ bitbake u-boot-adi -C compile
Finally, flash the u-boot LDR image into the SPI flash of SC5xx.
The ICC command can enable or disable a specific slave core. The SHARC core ids accepted by this command for SC5xx are 1 and 2, any other id value is ignored. The ICC message queue at the beginning of L2 SRAM is reset before enabling the SHARC cores.
sc # icc icc - Inter core communication interface Usage: icc icc enable <coreid> - enable coreid icc disable <coreid> - disable coreid
Enable the core control driver by using the below command:
$ bitbake linux-adi -c menuconfig CONFIG_CORE_CONTROL: ICC core control, control the DSP devices at the side of ARM Core, which provides some commands e.g. Start, Stop, and Set the vector value Symbol: CORE_CONTROL [=y] Type : bool Prompt: icc core control Location: -> Device Drivers -> Staging drivers (STAGING [=y]) -> icc driver (ICC [=y])
A new corectrl device would be created to allow Linux user to enable and disable the SHARC cores. See icc.h for macro values. The device, /dev/corectrl, supports the following ioctl requests:
Request | Description | Format |
---|---|---|
CMD_CORE_START | Start the specified core running from the programmed SVECT address. | int ioctl(<FD>,CMD_CORE_START, <COREID>); |
CMD_CORE_STOP | Stop the specified core by putting it back in reset. | int ioctl(<FD>, CMD_CORE_STOP, <COREID>); |
Both requests return 0 on success and -1 on failure.
An example to enable both cores is as follows:
#include <icc.h> ... int fd = open("/dev/corectrl", O_RDWR); if (fd < 0) { perror("Unable to open /dev/corectrl"); exit(1); } ... if (ioctl(fd, CMD_CORE_START, CCTRL_CORE1)) { perror("Unable to start Core 1"); exit(2); } if (ioctl(fd, CMD_CORE_START, CCTRL_CORE2)) { perror("Unable to start Core 2"); exit(3); }
The SHARC cores can be controlled from the Linux command line using the corecontrol utility. To use corecontrol, first add the package in local.conf:
$ vim /build/conf/local.conf IMAGE_INSTALL_append = " sc5xx-corecontrol"
With the corecontrol utility, sharc cores can be controlled to start or stop.
# corecontrol -h Valid options --start CORE_NUM --stop CORE_NUM # corecontrol --start 1 # corecontrol --stop 1
BACK TO Multi-Core Support