This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:control_sharc_cores [10 Dec 2020 10:46] – [Usage Example] Sunny Feng | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:control_sharc_cores [10 Dec 2020 10:46] (current) – [Example - Use corectrl device from source code] Sunny Feng | ||
---|---|---|---|
Line 67: | Line 67: | ||
:The number of the core to start or stop. Values accepted are CCTRL_CORE1 and CCTRL_CORE2. | :The number of the core to start or stop. Values accepted are CCTRL_CORE1 and CCTRL_CORE2. | ||
- | === Example | + | ==== Example: Use corectrl device from source code ==== |
An example to enable both cores is as follows: | An example to enable both cores is as follows: |