This is an old revision of the document!
This document talks about how we can load files on USB memory stick, into system RAM from u-boot. Here we take ADSP-SC573 board as example.
Connect USB stick to the USB OTG port, via the USB adapter cable, as following, and reset the board
Insert the USB memory stick into a Linux PC, you will see new items show up in /dev/sd*, as following:
$ ls /dev/sd* /dev/sda /dev/sda1 /dev/sda2 /dev/sda5 /dev/sdb /dev/sdb1
In this case the /dev/sdb is for the USB stick we just plugged in.
Caution : Please double check the device node newly created for your memory stick, otherwise serious damage like system permanent crash down happens!
The format a vfat partiton on it:
$ sudo mkfs.vfat /dev/sdb1 [sudo] password for ... mkfs.vfat 3.0.12 (29 Oct 2011)
$ sudo mount /dev/sdb1 /mnt $ cd build/tmp/deploy/images/adsp-sc573-ezkit $ sudo cp zImage /mnt/zImage $ sudo cp adsp-sc5xx-ramdisk-adsp-sc573-ezkit.cpio.gz.u-boot /mnt/ramdisk.cpio.gz.u-boot $ sudo cp sc573-ezkit.dtb /mnt $ sudo umount /mnt
Then plug the USB stick to the USB OTG port in board, via the USB adapter cable, and reset the board
Run “start usb” In the u-boot console:
sc # usb start (Re)start USB... USB0: scanning bus 0 for devices... 1 USB Device(s) found scanning usb for storage devices... 1 Storage Device(s) found
Run “fatls usb 0:1” In the u-boot console:
sc # fatls usb 0:1 12452384 zImage 10306 sc573-ezkit.dtb 2 file(s), 0 dir(s)
This shows the FAT files information in USB device 0 partition 1, with files we copied.
As example we load both the dtb, zImage and the ramdisk file into proper location.
Don't forget to change the file/dtb name and load address according to your board type (i.e. SC589-ezkit or SC584-ezkit or SC573-ezkit), otherwise it may not boot properly.
sc # fatload usb 0:1 0x84000000 sc573-ezkit.dtb reading sc573-ezkit.dtb 10306 bytes read in 30 ms (335 KiB/s) sc # fatload usb 0:1 0x82000000 zImage reading zImage 12452384 bytes read in 7772 ms (1.5 MiB/s)
Verify the read operation:
sc # bootz 0x82000000 - 0x84000000 ## Booting kernel from Legacy Image at 82000000 ... Image Name: Linux-4.0.0-ADI-1.1.0-00027-g5c7 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 12452320 Bytes = 11.9 MiB Load Address: 82008000 Entry Point: 82008000 Verifying Checksum ... OK ## Flattened Device Tree blob at 84000000 Booting using the fdt blob at 0x84000000 Loading Kernel Image ... OK Loading Device Tree to 8fe5d000, end 8fe62841 ... OK Starting kernel ... Booting Linux on physical CPU 0x0 Linux version 4.0.0-ADI-1.1.0-00027-g5c77b60 (i7@i7-OptiPlex-9010) (gcc version 4.8.3 (Analog Devices Inc. ARM Tools (e596c0da91703b047df99f5513e6 CPU: ARMv7 Processor [410fc051] revision 1 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: ADI sc57x-ezkit bootconsole [earlycon0] enabled Memory policy: Data cache writeback dump init clock rate CGU0_PLL 450 MHz CGU0_SYSCLK 225 MHz CGU0_CCLK 450 MHz CGU0_SYS0 112 MHz CGU0_DCLK 225 MHz CGU0_OCLK 150 MHz CGU0_SYS0 112 MHz Built 1 zonelists in Zone order, mobility grouping on. Total pages: 56896 Kernel command line: root=/dev/mtdblock2 rw rootfstype=jffs2 clkin_hz=(25000000) earlyprintk=serial,uart0,57600 console=ttySC0,57600 mem=224M PID hash table entries: 1024 (order: 0, 4096 bytes) Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Memory: 215024K/229376K available (3139K kernel code, 96K rwdata, 1184K rodata, 7736K init, 71K bss, 14352K reserved, 0K cma-reserved) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0xce800000 - 0xff000000 ( 776 MB) lowmem : 0xc0000000 - 0xce000000 ( 224 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .text : 0xc0008000 - 0xc044113c (4325 kB) .init : 0xc0442000 - 0xc0bd0000 (7736 kB) .data : 0xc0bd0000 - 0xc0be81e0 ( 97 kB) .bss : 0xc0be81e0 - 0xc0bfa098 ( 72 kB) NR_IRQS:16 nr_irqs:16 16 GIC CPU mask not found - kernel will fail to boot. GIC CPU mask not found - kernel will fail to boot. sched_clock: 32 bits at 112MHz, resolution 8ns, wraps every 38177486839ns Console: colour dummy device 80x30 Calibrating delay loop... 297.98 BogoMIPS (lpj=595968) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok Setting up static identity map for 0x822fdd48 - 0x822fdd7c devtmpfs: initialized do_initcall_level level 0 do_initcall_level level 1 VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1 pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 do_initcall_level level 2 DMA: preallocated 256 KiB pool for atomic coherent allocations do_initcall_level level 3 L2C: device tree omits to specify unified cache L2C-310 dynamic clock gating enabled, standby mode enabled L2C-310 cache controller enabled, 8 ways, 256 kB L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x06040000 sc57x_init: registering device resources sec init... enabled hw-breakpoint: Failed to enable monitor mode on CPU 0. ADI DMA2 Controller adi-dma2 31026180.dma: Invalid ADI DMA channel. adi-dma2: probe of 31026180.dma failed with error -2 adi-dma2 31026100.dma: Invalid ADI DMA channel. adi-dma2: probe of 31026100.dma failed with error -2 adi-dma2 30fff080.dma: Invalid ADI DMA channel. adi-dma2: probe of 30fff080.dma failed with error -2 adi-dma2 31026280.dma: Invalid ADI DMA channel. adi-dma2: probe of 31026280.dma failed with error -2 adi-dma2 31026200.dma: Invalid ADI DMA channel. adi-dma2: probe of 31026200.dma failed with error -2 adi-dma2 3109a000.dma: Invalid ADI DMA channel. adi-dma2: probe of 3109a000.dma failed with error -2 adi-dma2 3109a080.dma: Invalid ADI DMA channel. adi-dma2: probe of 3109a080.dma failed with error -2 adi-dma2 3109b000.dma: Invalid ADI DMA channel. adi-dma2: probe of 3109b000.dma failed with error -2 adi-dma2 3109b080.dma: Invalid ADI DMA channel. adi-dma2: probe of 3109b080.dma failed with error -2 DMA channel 40 is not registed DMA channel 39 is not registed do_initcall_level level 4 SCSI subsystem initialized i2c-bfin-twi 31001400.twi: Blackfin on-chip I2C TWI Contoller, regs_base@f4001400 i2c-bfin-twi 31001500.twi: Blackfin on-chip I2C TWI Contoller, regs_base@f4001500 i2c-bfin-twi 31001600.twi: Blackfin on-chip I2C TWI Contoller, regs_base@f4001600 pps_core: LinuxPPS API ver. 1 registered pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> PTP clock support registered do_initcall_level level 5 Switched to clocksource cs_gptimer NET: Registered protocol family 2 TCP established hash table entries: 2048 (order: 1, 8192 bytes) TCP bind hash table entries: 2048 (order: 1, 8192 bytes) TCP: Hash tables configured (established 2048 bind 2048) TCP: reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 do_initcall_level level 6 hw perfevents: enabled with armv7_cortex_a5 PMU driver, 3 counters available futex hash table entries: 256 (order: -1, 3072 bytes) jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. io scheduler noop registered (default) ADI serial driver adi-uart4.0: ttySC0 at MMIO 0x31003000 (irq = 20, base_baud = 7031250) is a ADI-UART4 console [ttySC0] enabled console [ttySC0] enabled bootconsole [earlycon0] disabled bootconsole [earlycon0] disabled adi-uart4.2: ttySC2 at MMIO 0x31003800 (irq = 60, base_baud = 7031250) is a ADI-UART4 loop: module loaded adi-spi3 3102e000.spi: registered ADI SPI controller spi0 adi-spi3 3102f000.spi: registered ADI SPI controller spi1 adi-spi3 31044000.spi: registered ADI SPI controller spi2 stmmaceth 3100c000.ethernet: no reset control found stmmac - user ID: 0x10, Synopsys ID: 0x37 Ring mode enabled DMA HW capability register supported Enhanced/Alternate descriptors Enabled extended descriptors RX Checksum Offload Engine supported (type 2) TX Checksum insertion supported Wake-Up On Lan supported Enable RX Mitigation via HW Watchdog Timer libphy: stmmac: probed eth0: PHY ID 20005c7a at 1 IRQ POLL (stmmac-0:01) active mousedev: PS/2 mouse device common for all mice i2c /dev entries driver adi_wdt: initialized: timeout=20 sec (nowayout=0) TCP: cubic registered NET: Registered protocol family 17 do_initcall_level level 7 ThumbEE CPU extension supported. Freeing unused kernel memory: 7736K (c0442000 - c0bd0000) Starting logging: OK Starting mdev... Starting watchdog... Initializing random number generator... random: dd urandom read with 8 bits of entropy available done. Starting network... /bin/sh: run-parts: not found ssh-keygen: generating new host keys: ED25519 Starting sshd: OK Starting inetd: OK
There are more command available for USB in u-boot:
sc # usb info 1: Mass Storage, USB Revision 2.0 - Generic USB Storage 000000009451 - Class: (from Interface) Mass Storage - PacketSize: 64 Configurations: 1 - Vendor: 0x05e3 Product 0x0723 Version 148.81 Configuration: 1 - Interfaces: 1 Bus Powered 500mA Interface: 0 - Alternate Setting 0, Endpoints: 2 - Class Mass Storage, Transp. SCSI, Bulk only - Endpoint 1 In Bulk MaxPacket 512 - Endpoint 2 Out Bulk MaxPacket 512
sc # usb storage Device 0: Vendor: Generic Rev: 9451 Prod: STORAGE DEVICE Type: Removable Hard Disk Capacity: 1897.0 MB = 1.8 GB (3885056 x 512)
sc # usb tree USB device tree: 1 Mass Storage (12 Mb/s, 500mA) Generic USB Storage 000000009451
sc # fatinfo usb 0:1 Interface: USB Device 0: Vendor: Generic Rev: 9451 Prod: STORAGE DEVICE Type: Removable Hard Disk Capacity: 1897.0 MB = 1.8 GB (3885056 x 512) Filesystem: FAT32 " "
MACHINE | DTB_FILE | FULL_FS_IMAGE | MINIMAL_FS_IMAGE | RAMDISK_FILE |
---|---|---|---|---|
adsp-sc589-mini | sc589-mini.dtb | adsp-sc5xx-full-adsp-sc589-mini.tar.xz | adsp-sc5xx-minimal-adsp-sc589-mini.tar.xz | adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz.u-boot |
adsp-sc589-ezkit | sc589-ezkit.dtb | adsp-sc5xx-full-adsp-sc589-ezkit.tar.xz | adsp-sc5xx-minimal-adsp-sc589-ezkit.tar.xz | adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz.u-boot |
adsp-sc584-ezkit | sc584-ezkit.dtb | adsp-sc5xx-full-adsp-sc584-ezkit.tar.xz | adsp-sc5xx-minimal-adsp-sc584-ezkit.tar.xz | adsp-sc5xx-ramdisk-adsp-sc584-ezkit.cpio.xz.u-boot |
adsp-sc573-ezkit | sc573-ezkit.dtb | adsp-sc5xx-full-adsp-sc573-ezkit.tar.xz | adsp-sc5xx-minimal-adsp-sc573-ezkit.tar.xz | adsp-sc5xx-ramdisk-adsp-sc573-ezkit.cpio.xz.u-boot |
Back To: Das U-boot