Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:tools-software:linux-software:libiio:clients:visual_analog [21 Jun 2019 21:22] – add note Robin Getz | resources:tools-software:linux-software:libiio:clients:visual_analog [29 Dec 2020 05:53] (current) – fix links Robin Getz |
---|
| |
===== About ===== | ===== About ===== |
IIO Plugin is a [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design-tools/visualanalog.html|Visual Analog]] component designed to create a communication channel between Visual Analog and the evaluation board attached to an embedded platform for the purpose of streaming data from the ADCs available on the board. The plugin can be used in conjunction with signal analysis components provided by Visual Analog in order to evaluate the performance of the board. | IIO Plugin is a [[adi>en/design-center/interactive-design-tools/visualanalog.html|Visual Analog]] component designed to create a communication channel between Visual Analog and the evaluation board attached to an embedded platform for the purpose of streaming data from the ADCs available on the board. The plugin can be used in conjunction with signal analysis components provided by Visual Analog in order to evaluate the performance of the board. |
| |
===== Installation ===== | ===== Installation ===== |
- Determine the IP address of the target by typing ''ifconfig'' in a terminal/console. | - Determine the IP address of the target by typing ''ifconfig'' in a terminal/console. |
PC side: | PC side: |
- Install [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design-tools/visualanalog.html|Visual Analog]] on your system. | - Install [[adi>en/design-center/interactive-design-tools/visualanalog.html|Visual Analog]] on your system. |
- Run the Visual Analog IIO Plugin installer available in the [[#downloads|Downloads ]] section. | - Run the Visual Analog IIO Plugin installer available in the [[#downloads|Downloads ]] section. |
- Fill the **Server IP Address** field of the plugin configuration panel, with the IP address of the target. | - Fill the **Server IP Address** field of the plugin configuration panel, with the IP address of the target. |
| |
====== User Guide ====== | ====== User Guide ====== |
* Run [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design tools/visualanalog.html|Visual Analog]]. | * Run [[adi>/en/design-center/interactive-design-tools/visualanalog.html|Visual Analog]]. |
* Choose **Blank Canvas** as a template. | * Choose **Blank Canvas** as a template. |
| |