Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:linux-software:libiio:clients:visual_analog [28 May 2015 17:14] – Update the download URL of the installer Dan Nechitaresources:tools-software:linux-software:libiio:clients:visual_analog [29 Dec 2020 05:53] (current) – fix links Robin Getz
Line 1: Line 1:
 ====== IIO Plugin for Visual Analog ====== ====== IIO Plugin for Visual Analog ======
-IIO Plugin is a [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design-tools/visualanalog.html|Visual Analog]] component designed to create a communication channel between Visual Analog and the evaluation board attached to an embedded platform for the purpose of streaming data from the ADCs available on the board. The plugin can be used in conjunction with signal analysis components provided by Visual Analog in order to evaluate the performance of the board. 
  
 +<WRAP important>
 +This software is [[wp>Deprecation|deprecated]] and is no longer supported/tested. It is described here for historical purposes only. If you have questions, please try things out with [[../../iio_oscilloscope|IIO Scope]], or ask questions on [[ez>linux-device-drivers/linux-software-drivers|EngineerZone]].
 +</WRAP>
 +
 +===== About =====
 +IIO Plugin is a [[adi>en/design-center/interactive-design-tools/visualanalog.html|Visual Analog]] component designed to create a communication channel between Visual Analog and the evaluation board attached to an embedded platform for the purpose of streaming data from the ADCs available on the board. The plugin can be used in conjunction with signal analysis components provided by Visual Analog in order to evaluate the performance of the board.
 +
 +===== Installation =====
 +The IIO plugin depends on the [[resources:tools-software:linux-software:libiio|libiio]] library which needs to be installed separately in order for the plugin to work.
 ====== Downloads ====== ====== Downloads ======
 <WRAP download> <WRAP download>
-  * [[http://swdownloads.analog.com/cse/va/VA_IIOPluginSetup.exe|IIO Plugin installer]]+  * [[http://swdownloads.analog.com/cse/va/VA_IIOPluginSetup.exe|IIO Plugin installer (old)]] 
 +  * {{:resources:tools-software:linux-software:libiio:clients:va_iiopluginsetup.zip|IIO Plugin for Visual Analog}} 
 +</WRAP> 
 + 
 +<WRAP round info 80%> 
 +  * The old plugin can be used by users that still run old versions of libiio on their targets. It also installs Libiio locally, next to the plugin. 
 +  * The new plugin works with Libiio 0.10 which needs to be installed separately. **First, look for 'LibIIO Setup x86' in 'Programs and Features' and uninstall it, then uninstall the old IIO plugin, if exists ** and then install the new one.
 </WRAP> </WRAP>
  
Line 14: Line 28:
 Target side: Target side:
   - Make sure the latest version of libiio is installed on target by following these [[/resources/tools-software/linux-software/libiio#building_on_the_linuxzynq_target|instructions]].   - Make sure the latest version of libiio is installed on target by following these [[/resources/tools-software/linux-software/libiio#building_on_the_linuxzynq_target|instructions]].
 +  - Determine the IP address of the target by typing ''ifconfig'' in a terminal/console.
 PC side: PC side:
-  - Install [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design-tools/visualanalog.html|Visual Analog]] on your system.+  - Install [[adi>en/design-center/interactive-design-tools/visualanalog.html|Visual Analog]] on your system.
   - Run the Visual Analog IIO Plugin installer available in the  [[#downloads|Downloads ]] section.   - Run the Visual Analog IIO Plugin installer available in the  [[#downloads|Downloads ]] section.
-  - Find out the IP address of the target by typing "ifconfig" in a terminal on the target side and use it to fill the **Server IP Address** field of the plugin configuration panel.+  - Fill the **Server IP Address** field of the plugin configuration panel, with the IP address of the target.
  
 ====== User Guide ====== ====== User Guide ======
-  * Run [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design tools/visualanalog.html|Visual Analog]].+  * Run [[adi>/en/design-center/interactive-design-tools/visualanalog.html|Visual Analog]].
   * Choose **Blank Canvas** as a template.   * Choose **Blank Canvas** as a template.
  
resources/tools-software/linux-software/libiio/clients/visual_analog.txt · Last modified: 29 Dec 2020 05:53 by Robin Getz