2022-05-06 14:35:15 URL: http://github.com/analogdevicesinc 200 OK
*** Updating linux_image_ADI-scripts BRANCH origin/master ***
HEAD is now at 47416bc update_tools: Add HWMON and examples to libiio builds
remote: Enumerating objects: 32, done.
remote: Counting objects: 100% (32/32), done.
remote: Compressing objects: 100% (16/16), done.
remote: Total 32 (delta 16), reused 30 (delta 16), pack-reused 0
Unpacking objects: 100% (32/32), 7.80 KiB | 133.00 KiB/s, done.
From https://github.com/analogdevicesinc/linux_image_ADI-scripts
* [new branch] add_2021_R1_release -> origin/add_2021_R1_release
47416bc..425510e master -> origin/master
+ c989e52...4bf27ce rpi_boot_files -> origin/rpi_boot_files (forced update)
*** Building linux_image_ADI-scripts ***
./adi_update_tools.sh has been updated, switching to new one
2022-05-06 14:35:18 URL: http://github.com/analogdevicesinc 200 OK
*** Updating linux_image_ADI-scripts BRANCH origin/master ***
HEAD is now at 425510e adi_update_boot.sh: Replace windows carrige/return
*** Building linux_image_ADI-scripts ***
./adi_update_tools.sh script is the same, continuing
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
Note, selecting 'libncurses-dev' instead of 'ncurses-dev'
bison is already the newest version (2:3.7.5+dfsg-1).
flex is already the newest version (2.6.4-8).
libaio-dev is already the newest version (0.3.112-9+rpi1).
libavahi-client-dev is already the newest version (0.8-5).
libavahi-common-dev is already the newest version (0.8-5).
libcdk5-dev is already the newest version (5.0.20180306-3).
libcurl4-openssl-dev is already the newest version (7.74.0-1.3+deb11u1).
libfftw3-dev is already the newest version (3.3.8-2).
libgtkdatabox-dev is already the newest version (1:0.9.3.1-2).
libjansson-dev is already the newest version (2.13.1-1.1).
libmatio-dev is already the newest version (1.5.19-2).
libncurses-dev is already the newest version (6.2+20201114-2).
libserialport-dev is already the newest version (0.1.1-4).
libxml2 is already the newest version (2.9.10+dfsg-6.7+deb11u1).
libxml2-dev is already the newest version (2.9.10+dfsg-6.7+deb11u1).
cmake is already the newest version (3.18.4-2+rpt1+rpi1).
libgtk2.0-dev is already the newest version (2.24.33-2+rpt1).
0 upgraded, 0 newly installed, 0 to remove and 49 not upgraded.
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
evtest is already the newest version (1:1.34-1).
gpsd is already the newest version (3.22-4).
gpsd-clients is already the newest version (3.22-4).
u-boot-tools is already the newest version (2021.01+dfsg-5+rpi1).
0 upgraded, 0 newly installed, 0 to remove and 49 not upgraded.
Cannot read environment, using default
Cannot read default environment from file
sed: can't read /etc/update-motd.d/10-help-text: No such file or directory
make: *** No rule to make target 'clean'. Stop.
install -d /usr/local/bin
install ./*.sh /usr/local/bin/
/bin/sh usb-gadget-service/install_gt.sh
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
libconfig-dev is already the newest version (1.5-0.4).
Already up to date.
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for a thread-safe mkdir -p... /usr/bin/mkdir -p
checking for gawk... no
checking for mawk... mawk
checking whether make sets $(MAKE)... yes
checking whether make supports nested variables... yes
checking for gcc... gcc
checking whether the C compiler works... yes
checking for C compiler default output file name... a.out
checking for suffix of executables...
checking whether we are cross compiling... no
checking for suffix of object files... o
checking whether we are using the GNU C compiler... yes
checking whether gcc accepts -g... yes
checking for gcc option to accept ISO C89... none needed
checking whether gcc understands -c and -o together... yes
checking whether make supports the include directive... yes (GNU style)
checking dependency style of gcc... gcc3
checking for g++... g++
checking whether we are using the GNU C++ compiler... yes
checking whether g++ accepts -g... yes
checking dependency style of g++... gcc3
checking for ar... ar
checking the archiver (ar) interface... ar
checking for pkg-config... /usr/bin/pkg-config
checking pkg-config is at least version 0.9.0... yes
checking for libconfig >= 1.4... yes
checking for libconfig >= 1.5... yes
checking build system type... armv7l-unknown-linux-gnueabihf
checking host system type... armv7l-unknown-linux-gnueabihf
checking how to print strings... printf
checking for a sed that does not truncate output... /usr/bin/sed
checking for grep that handles long lines and -e... /usr/bin/grep
checking for egrep... /usr/bin/grep -E
checking for fgrep... /usr/bin/grep -F
checking for ld used by gcc... /usr/bin/ld
checking if the linker (/usr/bin/ld) is GNU ld... yes
checking for BSD- or MS-compatible name lister (nm)... /usr/bin/nm -B
checking the name lister (/usr/bin/nm -B) interface... BSD nm
checking whether ln -s works... yes
checking the maximum length of command line arguments... 1572864
checking how to convert armv7l-unknown-linux-gnueabihf file names to armv7l-unknown-linux-gnueabihf format... func_convert_file_noop
checking how to convert armv7l-unknown-linux-gnueabihf file names to toolchain format... func_convert_file_noop
checking for /usr/bin/ld option to reload object files... -r
checking for objdump... objdump
checking how to recognize dependent libraries... pass_all
checking for dlltool... no
checking how to associate runtime and link libraries... printf %s\n
checking for archiver @FILE support... @
checking for strip... strip
checking for ranlib... ranlib
checking command to parse /usr/bin/nm -B output from gcc object... ok
checking for sysroot... no
checking for a working dd... /usr/bin/dd
checking how to truncate binary pipes... /usr/bin/dd bs=4096 count=1
checking for mt... mt
checking if mt is a manifest tool... no
checking how to run the C preprocessor... gcc -E
checking for ANSI C header files... yes
checking for sys/types.h... yes
checking for sys/stat.h... yes
checking for stdlib.h... yes
checking for string.h... yes
checking for memory.h... yes
checking for strings.h... yes
checking for inttypes.h... yes
checking for stdint.h... yes
checking for unistd.h... yes
checking for dlfcn.h... yes
checking for objdir... .libs
checking if gcc supports -fno-rtti -fno-exceptions... no
checking for gcc option to produce PIC... -fPIC -DPIC
checking if gcc PIC flag -fPIC -DPIC works... yes
checking if gcc static flag -static works... yes
checking if gcc supports -c -o file.o... yes
checking if gcc supports -c -o file.o... (cached) yes
checking whether the gcc linker (/usr/bin/ld) supports shared libraries... yes
checking whether -lc should be explicitly linked in... no
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
checking if libtool supports shared libraries... yes
checking whether to build shared libraries... yes
checking whether to build static libraries... yes
checking how to run the C++ preprocessor... g++ -E
checking for ld used by g++... /usr/bin/ld
checking if the linker (/usr/bin/ld) is GNU ld... yes
checking whether the g++ linker (/usr/bin/ld) supports shared libraries... yes
checking for g++ option to produce PIC... -fPIC -DPIC
checking if g++ PIC flag -fPIC -DPIC works... yes
checking if g++ static flag -static works... yes
checking if g++ supports -c -o file.o... yes
checking if g++ supports -c -o file.o... (cached) yes
checking whether the g++ linker (/usr/bin/ld) supports shared libraries... yes
checking dynamic linker characteristics... (cached) GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking for doxygen... /usr/bin/doxygen
checking for perl... /usr/bin/perl
checking for dot... /usr/bin/dot
checking for latex... no
configure: WARNING: latex not found - will not generate doxygen PostScript documentation
checking for makeindex... no
checking for dvips... no
checking for egrep... /usr/bin/egrep
checking for pdflatex... no
configure: WARNING: pdflatex not found - will not generate doxygen PDF documentation
checking for makeindex... no
checking for egrep... (cached) /usr/bin/egrep
DX_FLAG_doc=1
DX_FLAG_dot=1
DX_FLAG_man=0
DX_FLAG_html=1
DX_FLAG_chm=0
DX_FLAG_chi=0
DX_FLAG_rtf=0
DX_FLAG_xml=0
DX_FLAG_pdf=0
DX_FLAG_ps=0
DX_ENV= SRCDIR='.' PROJECT='libusbgx' DOCDIR='doxygen-doc' VERSION='0.2.0' PERL_PATH='/usr/bin/perl' HAVE_DOT='YES' DOT_PATH='/usr/bin' GENERATE_MAN='NO' GENERATE_RTF='NO' GENERATE_XML='NO' GENERATE_HTMLHELP='NO' GENERATE_CHI='NO' GENERATE_HTML='YES' GENERATE_LATEX='NO'
checking that generated files are newer than configure... done
configure: creating ./config.status
config.status: creating Makefile
config.status: creating src/Makefile
config.status: creating examples/Makefile
config.status: creating include/usbg/usbg_version.h
config.status: creating libusbgx.pc
config.status: creating doxygen.cfg
config.status: creating LibUsbgxConfig.cmake
config.status: executing depfiles commands
config.status: executing libtool commands
make[1]: warning: jobserver unavailable: using -j1. Add '+' to parent make rule.
make[1]: Entering directory '/usr/local/src/libusbgx'
Making all in src
....
*** Building libiio ***
-- cmake version: 3.18.4
-- The C compiler identification is GNU 10.2.1
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /usr/bin/cc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Performing Test HAS_WPEDANTIC
-- Performing Test HAS_WPEDANTIC - Success
-- Performing Test HAS_WSHADOW
-- Performing Test HAS_WSHADOW - Success
-- Looking for strdup
-- Looking for strdup - found
-- Looking for strndup
-- Looking for strndup - found
-- Looking for strerror_r
-- Looking for strerror_r - found
-- Looking for newlocale
-- Looking for newlocale - found
-- Looking for pthread_setname_np
-- Looking for pthread_setname_np - found
-- Looking for in6addr_any
-- Looking for in6addr_any - found
-- Looking for libusb-1.0 : Found
-- Looking for libusb_get_version
-- Looking for libusb_get_version - found
-- Found Git: /usr/bin/git (found version "2.30.2")
-- Looking for libserialport : Found
-- Building with Network back end support
-- Performing Test HAS_O_TMPFILE
-- Performing Test HAS_O_TMPFILE - Success
-- Performing Test WITH_NETWORK_EVENTFD
-- Performing Test WITH_NETWORK_EVENTFD - Success
-- Performing Test HAS_PIPE2
-- Performing Test HAS_PIPE2 - Success
-- Building with Avahi, a DNS SD implementation
-- Found LibXml2: /usr/lib/arm-linux-gnueabihf/libxml2.so (found version "2.9.10")
-- Looking for CDK_CSTRING2
-- Looking for CDK_CSTRING2 - found
-- bin= lib= inc=
-- Found Python: /usr/bin/python3.9 (found version "3.9.2") found components: Interpreter
-- new
-- Python_EXECUTABLE /usr/bin/python3.9
-- Found Python: Building bindings
-- Found BISON: /usr/bin/bison (found version "3.7.5")
-- Found FLEX: /usr/bin/flex (found version "2.6.4")
-- Looking for sys/types.h
-- Looking for sys/types.h - found
-- Looking for stdint.h
-- Looking for stdint.h - found
-- Looking for stddef.h
-- Looking for stddef.h - found
-- Check size of struct usb_functionfs_descs_head_v2
-- Check size of struct usb_functionfs_descs_head_v2 - done
-- Configuring done
-- Generating done
-- Build files have been written to: /usr/local/src/libiio/build
....
Building libiio target finished Successfully
*** Updating libad9361-iio BRANCH origin/2019_R2 ***
Previous HEAD position was fd44358 Fix flags for FMComms5 python tests
HEAD is now at be7eb02 Update HW test to use environmental variables
remote: Enumerating objects: 3, done.
remote: Counting objects: 100% (3/3), done.
remote: Total 3 (delta 2), reused 3 (delta 2), pack-reused 0
Unpacking objects: 100% (3/3), 601 bytes | 120.00 KiB/s, done.
From https://github.com/analogdevicesinc/libad9361-iio
* [new branch] 2021_R1 -> origin/2021_R1
* [new branch] staging/ci-update -> origin/staging/ci-update
*** Building libad9361-iio ***
-- The C compiler identification is GNU 10.2.1
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Check for working C compiler: /usr/bin/cc - skipped
-- Detecting C compile features
-- Detecting C compile features - done
-- Found Git: /usr/bin/git (found version "2.30.2")
-- Found Doxygen: /usr/bin/doxygen (found version "1.9.1") found components: doxygen dot
-- Using default dependencies for packaging
-- Package dependencies: libc6-dev (>= 2.19)
-- Configuring done
-- Generating done
-- Build files have been written to: /usr/local/src/libad9361-iio/build
....
Building libad9361-iio target finished Successfully
*** Updating iio-oscilloscope BRANCH origin/2019_R2 ***
Previous HEAD position was fb9ec84 plugins: adrv9002: improve temperature reporting
HEAD is now at 177dd7d filters: add adrv9002 new API profiles
rm -rf /usr/local/lib/osc /usr/local/share/osc /usr/local/bin/osc /usr/local/lib/libosc.so
xdg-icon-resource uninstall --noupdate --size 16 adi-osc
xdg-icon-resource uninstall --noupdate --size 32 adi-osc
xdg-icon-resource uninstall --noupdate --size 64 adi-osc
xdg-icon-resource uninstall --noupdate --size 128 adi-osc
....