This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-software:iio_oscilloscope [28 Jul 2017 13:51] – [Linux/OS X] Lars-Peter Clausen | resources:tools-software:linux-software:iio_oscilloscope [04 Apr 2018 19:22] – Updated to heading of provided waveforms Travis Collins | ||
---|---|---|---|
Line 208: | Line 208: | ||
To do so, right-click on the name of the device used for capture, and select **Trigger settings**. | To do so, right-click on the name of the device used for capture, and select **Trigger settings**. | ||
The pop-up window that will open will allow you to configure the channel used for the trigger, as well as the trigger level and edge. | The pop-up window that will open will allow you to configure the channel used for the trigger, as well as the trigger level and edge. | ||
+ | |||
+ | ====== Provided Waveforms ====== | ||
+ | |||
+ | Several waveforms are provided with the application for demonstration purposes, which can be loaded into different devices. | ||
+ | |||
====== Source code ====== | ====== Source code ====== | ||