This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-software:iio_oscilloscope [06 Mar 2017 22:40] – add page Robin Getz | resources:tools-software:linux-software:iio_oscilloscope [28 Jul 2017 13:51] – [Linux/OS X] Lars-Peter Clausen | ||
---|---|---|---|
Line 18: | Line 18: | ||
To build on a host, do not use the script, you **must**: | To build on a host, do not use the script, you **must**: | ||
- | - make sure the following libraries are installed. This list is maintained in the '' | + | - make sure the following libraries are installed. This list is maintained in the '' |
+ | > **apt-get -y install libglib2.0-dev libgtk2.0-dev libgtkdatabox-dev libmatio-dev libfftw3-dev libxml2 libxml2-dev bison flex libavahi-common-dev libavahi-client-dev libcurl4-openssl-dev libjansson-dev cmake libaio-dev** | ||
+ | </ | ||
- build **and install** the libiio library, by following these [[libiio# | - build **and install** the libiio library, by following these [[libiio# | ||
+ | - build **and install** the libad9361-iio library, by following these [[: | ||
- download the source < | - download the source < | ||
> **git clone https:// | > **git clone https:// |