Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:tools-software:linux-software:iio_oscilloscope [08 May 2015 10:58] – [Main Window] Paul Cercueil | resources:tools-software:linux-software:iio_oscilloscope [10 Jul 2015 17:01] – [Main Window] Lucian Sin |
---|
**Debug** Plugin: Is a tool for device debugging. Since "normal" users should not be doing this, features on this tab may not work unless you have started the ''osc'' application as root (try ''sudo osc'' in a terminal). | **Debug** Plugin: Is a tool for device debugging. Since "normal" users should not be doing this, features on this tab may not work unless you have started the ''osc'' application as root (try ''sudo osc'' in a terminal). |
| |
* **Device Selection:** Sets the active device. Once a device is selected any other information displayed in the plugin related to this particular device. | * **Device Selection:** Sets the active device. Once a device is selected any other information displayed in the plugin is related to this particular device. |
* **IIO Device Attributes:** Allows Read/Write operation for the attributes of a device. | * **IIO Device Attributes:** Allows Read/Write operation for the attributes of a device. |
* **Register:** Provides low level access to the registers of the device. | * **Register:** Provides low level access to the registers of the device. |