This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-software:iio_oscilloscope [02 Mar 2015 23:11] – [Installation] Robin Getz | resources:tools-software:linux-software:iio_oscilloscope [21 Apr 2015 14:04] – [Capture Window] Paul Cercueil | ||
---|---|---|---|
Line 11: | Line 11: | ||
==== Windows ==== | ==== Windows ==== | ||
- | <WRAP round download | + | <WRAP round download> |
* **IIO Oscilloscope (OSC) for Win32 & Win64 (2014_R2 Alpha Pre-Release) ** | * **IIO Oscilloscope (OSC) for Win32 & Win64 (2014_R2 Alpha Pre-Release) ** | ||
* Download: [[http:// | * Download: [[http:// | ||
Line 187: | Line 187: | ||
Click on File→Save As to open the dialog needed to save the data. | Click on File→Save As to open the dialog needed to save the data. | ||
- | \\ \\ \\ \\ \\ \\ | + | \\ \\ \\ \\ |
- | == Channel Settings == | + | === Channel Settings |
{{ : | {{ : | ||
Line 199: | Line 199: | ||
The settings can be applied only in Time domain. | The settings can be applied only in Time domain. | ||
- | \\ \\ | + | \\ |
+ | === Trigger settings === | ||
+ | {{ : | ||
+ | |||
+ | In time domain, it is possible to select a capture channel as the trigger source of the oscilloscope. | ||
+ | To do so, right-click on the name of the device used for capture, and select **Trigger settings**. | ||
+ | The pop-up window that will open will allow you to configure the channel used for the trigger, as well as the trigger level and edge. | ||
====== Source code ====== | ====== Source code ====== | ||