The AD936X plugin (formerly known as the FMComms2/3/4 Plugin) works with the IIO Oscilloscope. You always use the latest version if possible. Changing any field will immediately write changes which have been made to the AD936X settings to the hardware, and then read it back to make sure the setting is valid. If you want to set something that the GUI changes to a different number, that either means that GUI is rounding (sorry), or the hardware (either the AD9361 or the FPGA fabric) does not support that mode/precision.
If you want to go play with /sys/bus/iio/devices/….
and manipulate the devices behind the back of the GUI, it's still possible to see the settings by clicking the “refresh” button at the bottom of the GUI.
If you think the device has a setting that isn't managed by this tab, check out the AD936X Advanced Plugin for the IIO Oscilloscope.
The AD936X view is divided in four sections:
The plugin provides several options on how the transmitted data is generated.I
It is possible to either use the built-in two tone Direct Digital Synthesizer (DDS) to transmit a bi-tonal signal on channels I and Q of the DAC. Or it is possible to use the Direct Memory Access (DMA) facility to transmit custom data that you have stored in a file.
This can be achieved by selecting one of the following options listed by the DDS Mode:
In One CW Tone mode one continuous wave (CW) tone will be outputted. The plugin displays the controls to set the Frequency, Amplitude and Phase for just one tone and makes sure that the amplitude of the other tone is set to 0. The resulting signal will be outputted on the Channel I of the DAC and the exact same signal but with a difference in phase of 90 degrees will be outputted on the Channel Q of the DAC.
In Two CW Tone mode two continuous wave (CW) tones will be outputted. The plugin displays the controls to set the frequencies F1 and F2, amplitudes A1 and A2, phases P1 and P2 for the two tones. The resulting signal will be outputted on the Channel I of the DAC and the exact same signal but with a difference in phase of 90 degrees will be outputted on the Channel Q of the DAC.
In Independent I/Q Control the plugin displays the controls to set the frequencies, amplitudes and phases for the two tones that will be outputted on channel I and additionally it allows for the two tones that will be outputted on channel Q of the DAC to be configured independently.
Note: The bi-tonal signal (T) is defined as the sum of two tones:
T(t) = A1 * sin(2 * π * F1 * t + P1) + A2 * sin(2 * π * F2 * t + P2),
where A-amplitude, F-frequency, P-phase of a tone.
The file selector under the File Selection section is used to locate and choose the desired data file. Under the DAC Channels section the enabled channels will be used to transmit the data stored in the file. To finalize the process, a click on the Load button is required.
Restrictions:
In this mode both DDS and DMA are disabled causing the DAC channels to stop transmitting any data.
Upon pressing Reload Settings button the values will be reloaded with the corresponding driver values. Useful in scenarios where the diver values get changed outside this plugin (e.g with the use of Debug plugin) and a refresh on plugin's values is needed.
Some plugin values will be rounded to the nearest value supported by the hardware.