This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-software:colorimeter [29 May 2015 14:52] – [Source code] Lars-Peter Clausen | resources:tools-software:linux-software:colorimeter [24 May 2018 13:35] (current) – Add an important note to close iio-osc before starting the app. Istvan Csomortani | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0363 Colorimeter Application User Guide ====== | ====== CN0363 Colorimeter Application User Guide ====== | ||
+ | ===== Starting the Application ===== | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The CN0363 Colorimeter Application can be launched from the top-left **" | ||
+ | |||
+ | <WRAP clear></ | ||
===== Analyzing a Sample ===== | ===== Analyzing a Sample ===== | ||
Line 12: | Line 21: | ||
==== Analyze Sample ==== | ==== Analyze Sample ==== | ||
- | Clicking the **Analyze Sample** button will perform | + | Clicking the **Analyze Sample** button will perform |
Once the analyzing process has finished it is also possible to either try to match the sample to a existing sample from the sample library or save the sample into the sample library for future use. | Once the analyzing process has finished it is also possible to either try to match the sample to a existing sample from the sample library or save the sample into the sample library for future use. | ||
Line 48: | Line 57: | ||
{{ : | {{ : | ||
- | The sample library allows to manage and compare previously saved sample data. On the left side is a list of all samples. On the right side the absorbence | + | The sample library allows to manage and compare previously saved sample data. On the left side is a list of all samples. On the right side the absorbance |
Samples can also be removed from the library by selecting the sample and then clicking the **Remove** button. A sample that has been removed from the library can not be restored. | Samples can also be removed from the library by selecting the sample and then clicking the **Remove** button. A sample that has been removed from the library can not be restored. | ||
Line 57: | Line 66: | ||
{{ : | {{ : | ||
- | For optimum performance it is necessary to calibrate the application to the connected board and the environment. This calibration can be performed in the calibration dialog which can be opened | + | For optimum performance it is necessary to calibrate the application to the connected board and the environment. This calibration can be performed in the calibration dialog which can be opened |
Calibration must be performed with distilled water in both the reference and the sample probes. It is also recommended that during calibration the photo-diodes are shielded from ambient light. | Calibration must be performed with distilled water in both the reference and the sample probes. It is also recommended that during calibration the photo-diodes are shielded from ambient light. | ||
Start the automatic calibration procedure in the software; from the Menu | Start the automatic calibration procedure in the software; from the Menu | ||
- | bar, open the **Calibration** dialog box, and click **Calibrate**.Once the calibration is done the calibration values will be updated. | + | bar, open the **Calibration** dialog box, and click **Calibrate**. Once the calibration is done the calibration values will be updated. |
It is also possible to save the current calibration data for later use by clicking the **Export** button or to load previously saved calibration data by clicking the **Import** button. | It is also possible to save the current calibration data for later use by clicking the **Export** button or to load previously saved calibration data by clicking the **Import** button. | ||
Line 75: | Line 84: | ||
**Install colorimeter application** | **Install colorimeter application** | ||
< | < | ||
- | < | + | < |
- | $ git clone https:// | + | |
Cloning into ' | Cloning into ' | ||
remote: Counting objects: 65, done. | remote: Counting objects: 65, done. | ||
Line 109: | Line 117: | ||
xdg-icon-resource install --noupdate --size 32 ./ | xdg-icon-resource install --noupdate --size 32 ./ | ||
xdg-icon-resource install --size 64 ./ | xdg-icon-resource install --size 64 ./ | ||
- | xdg-desktop-menu install adi-colorimeter.desktop | + | xdg-desktop-menu install adi-colorimeter.desktop</ |
- | </ | + | |
</ | </ | ||
</ | </ | ||
Line 116: | Line 123: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | * [[adi> | + | * [[adi> |
===== More Information ===== | ===== More Information ===== | ||
* [[: | * [[: |