This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-software:colorimeter [29 Feb 2016 10:36] – syntax correction Mihai Ionut Suciu | resources:tools-software:linux-software:colorimeter [29 Feb 2016 10:45] – syntax correction Mihai Ionut Suciu | ||
---|---|---|---|
Line 64: | Line 64: | ||
{{ : | {{ : | ||
- | For optimum performance it is necessary to calibrate the application to the connected board and the environment. This calibration can be performed in the calibration dialog which can be opened | + | For optimum performance it is necessary to calibrate the application to the connected board and the environment. This calibration can be performed in the calibration dialog which can be opened |
Calibration must be performed with distilled water in both the reference and the sample probes. It is also recommended that during calibration the photo-diodes are shielded from ambient light. | Calibration must be performed with distilled water in both the reference and the sample probes. It is also recommended that during calibration the photo-diodes are shielded from ambient light. |