This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-software:build-the-zynq-boot-image [24 Sep 2019 17:16] – Added cygwin specific configuration Adrian Costina | resources:tools-software:linux-software:build-the-zynq-boot-image [20 Mar 2023 12:38] (current) – Mention Vitis and .xsa instead of SDK and .hdf Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== How to build the Zynq boot image BOOT.BIN ====== | ====== How to build the Zynq boot image BOOT.BIN ====== | ||
- | The boot image BOOT.BIN is build using the bootgen tool which requires several input files.\\ | + | The boot image BOOT.BIN is built using the bootgen tool which requires several input files.\\ |
- | Instructions on how to build the Hardware Description File (HDF) handover file can be found here: | + | Instructions on how to build the Xilinx Shell Archive |
- | * [[resources/ | + | * [[resources/ |
Line 16: | Line 16: | ||
===== Use script to build BOOT.BIN ===== | ===== Use script to build BOOT.BIN ===== | ||
- | For ease of use we provide a bash shell script which allows building BOOT.BIN from system_top.hdf and u-boot.elf | + | For ease of use, we provide a bash shell script which allows building BOOT.BIN from system_top.xsa and u-boot.elf |
==== Download ==== | ==== Download ==== | ||
Line 34: | Line 34: | ||
< | < | ||
- | usage: build_boot_bin.sh system_top.hdf u-boot.elf [output-archive] | + | usage: build_boot_bin.sh system_top.xsa u-boot.elf [output-archive] |
</ | </ | ||
- | * Path to '' | + | * Path to '' |
- | * An optionally 3rd '' | + | * An optionally 3rd '' |
- | * Build output is located in a local directory named: output_boot_bin. | + | * Build output is located in a local directory named: output_boot_bin |
- | * This script requires Xilinx | + | * This script requires Xilinx |
* A simple way is to source vivado settings[32|64].sh: | * A simple way is to source vivado settings[32|64].sh: | ||
< | < | ||
- | $ source / | + | $ source / |
</ | </ | ||
Line 49: | Line 49: | ||
< | < | ||
- | export PATH=$PATH:/ | + | export PATH=$PATH:/ |
- | export PATH=$PATH:/ | + | export PATH=$PATH:/ |
</ | </ | ||
+ | There is also a version of script that works in Windows Powershell: [[ https:// | ||
< | < | ||
For those who don't want to build u-boot themselves.\\ | For those who don't want to build u-boot themselves.\\ | ||
- | The **u-boot.elf** can be extracted from the project folder on the [[resources/tools-software/linux-software/ | + | The **u-boot.elf** can be extracted from the project folder on the [[:resources:tools-software:linux-software: |
</ | </ |